RT KERNEL

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

RT KERNEL

1,002 次查看
Subhani7
Contributor II

Hi Team,

I am using 

LLDPUG
Layerscape Linux Distribution POC User Guide
Rev. L5.15.71-2.2.0

I need to Upgrade to RT kernel, How can i change linux-qoriq to RT kernel.

facing below issue, Can i change the git link in linux-qoriq recipe.
Is there any way ?

labuser@testing:~/LLDP_MP12/LINUX/target/yocto/build_lx2160ardb-rev2$ bitbake linux-yocto-rt
Loading cache: 100% |#############################################################################################| Time: 0:00:01Loaded 4805 entries from dependency cache.
Parsing recipes: 100% |###########################################################################################| Time: 0:00:01Parsing of 3229 .bb files complete (3226 cached, 3 parsed). 4808 targets, 599 skipped, 9 masked, 0 errors.
ERROR: Nothing PROVIDES 'linux-yocto-rt'
linux-yocto-rt was skipped: incompatible with machine lx2160ardb-rev2 (not in COMPATIBLE_MACHINE)
linux-yocto-rt was skipped: incompatible with machine lx2160ardb-rev2 (not in COMPATIBLE_MACHINE)

Regards
Subhani

0 项奖励
回复
1 回复

976 次查看
Oswalag
NXP TechSupport
NXP TechSupport

Hello,

Please refer to the following community post:

preempt-rt activation using bitbake

Have a nice day!

0 项奖励
回复