RMII configuration in P1013

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

RMII configuration in P1013

2,447 次查看
somyaaggarwal08
Contributor II

Hi,

I have a board based on p1013 processor. I have a phy device connected to etsec2 through rmii interface.I want to configure etsec2 in rmii mode from uboot. I have set ETSEC CNTRL as 0x1004 and MACCFG2 as 0x7105 . When i ping host pc from board i get ping failed , host is not alive. The MIB registers like Transmit bye counters and Receive byte counters remain zero during ping. However the physical link shows up at speed 100mbps and full duplex mode. Is there any other rmii configuration  which i may be missing upon?

0 项奖励
回复
5 回复数

2,321 次查看
somyaaggarwal08
Contributor II

Hi,

The problem got resolved. Thank you for the useful information

0 项奖励
回复

2,321 次查看
somyaaggarwal08
Contributor II

Hi,

 eTSEC2_MACCFG1 is 0x5.

In RMII mode  we are using shared reference clock between transmit and receive. We have also  probed the tx clk as 50Mhz

0 项奖励
回复

2,321 次查看
ufedor
NXP Employee
NXP Employee

What is eTSEC2_ECNTRL value?

What is GUTs_PORDEVSR value?

Ensure that cfg_tsec2_prtc is pulled low and cfg_serdes_ports[0:4] does not select SGMII2.

0 项奖励
回复

2,321 次查看
somyaaggarwal08
Contributor II

Hi ufedor

eTSEC2_ECNTRL is 0x100c

GUTs_PORDEVSR is 0x1b5c0040

I am getting error "eSEC2: tsec: tx error"

We have ensured that cfg_tsec2_prtc is pulled low and cfg_serdes_ports[0:4] does not select SGMII2 (10111)

0 项奖励
回复

2,321 次查看
ufedor
NXP Employee
NXP Employee

What is the eTSEC2_MACCFG1 value?

Ensure that TX_CLK and RX_CLK are applied to the processor.

0 项奖励
回复