RCPM Doze/Wake-Up features buggy on P4080?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RCPM Doze/Wake-Up features buggy on P4080?

5,049 Views
renatomancuso
Contributor I

We use a Freescale P4080 with major revision number 2, minor rev. number 0. I will refer to two pieces of documentation for the P4080:

[1] The "P4080 QorIQ Integrated Multicore Communication Processor Family Reference Manual" (P4080RM) - we have Rev. 0, 04/2011

[2] The "P4080 Advanced QorIQ Debug and Performance Monitoring Reference Manual" (P4080DEBUGRM) - we have Rev. E, 06/2011

The question regards the functionality of the Run Control and Power Management Unit (RCPM). This unit has two interfaces: one for power management that is described in [1] at Chapter 26; and a second one that performs run control in response to platform events, mapped in DCSR space and described in [2] in Section 11.

Out of all the possible power states that are available to be selected in the RCPM, we are only interested in Full-on mode and Dozing mode for power-saving techniques.

According to the two pieces of documentation, and following the description of the RCPM in [2], the registers CGACRE 0-15 can be used to select an run control action in response to a SCU event.

Each of the CGACRE 0-15 registers exposes a PCAC field for passive core action control as well as an ICAC field for intrusive core action control.

First of all, the ICAC field in the P4080DEBUGRM Rev 0 is not directly documented, but only mentioned in Chapter 12, Section 12.5.7.1 and Section 12.5.7.2. After some investigation, I have found that the ICAC field corresponds to bits 24-27 of the CGACRE registers. Here is the mapping of ICAC value to action, again according to the observed behavior of the platform:

1. ICAC = 0010 -> Cores in corresponding core group are put in "Debug Halted"

2. ICAC = 0100 -> Cores in corresponding core group are requested to enter "Dozing" status

3. ICAC = 0001 -> Cores in corresponding core group are requested to exit "Dozing" status and resume Full-on mode operations

Now, I configure two SCU, say SCU0 and SCU1 so that each generates a non-sticky event roughly every 2 seconds, with a phase of 1 second, leading to the sequence:

Time 0s: SCU0 event; Time 1s SCU1 event; Time 2s SCU0 event; Time 3s SCU1 event; ...

I configure CGACRE0 (in response to a SCU0 event) to send a enter-dozing request to Core 0.

Similarly, I configure CGACRE1 (in response to a SCU1 event) to send a exit-dozing request to Core 0.

However, the behavior of the system is not the one expected, because: at Time 0, Core 0 correctly enters dozing; at Time 1, Core 0 resumes operations exiting from dozing status; at Time 2, however, Core 0 does not enter dozing anymore and any other dozing request from the RCPM unit is ignored by the core.

Note 1: If the ICAC field in the CGACRE1 (in response to SCU1 events) is cleared, indicating no action, requests of dozing from SCU0 are processed correctly.

Note 2: Even if the configuration of SCU0 is altered so that after firing a first event, no further events are generated, programming the ICAC field of CGACRE0 with "0001" is enough to prevent any dozing request to be successful.

Note 3: In our default configuration, the field MSR[DE]=0 and DBCR[IDM]=1. Hence, an action from SCU1 triggers the occurrence of a Imprecise Debug Event (IDE). However, if DBCR[IDM]=0 (hence suppressing the occurrence of the IDE condition) the behavior of the system does not change.

In summary, we would like to know whether this is an "expected" behavior of the platform or rather a problem of the particular chip revision that we are using (P4080 Rev. 2.0).

0 Kudos
Reply
6 Replies

4,635 Views
renatomancuso
Contributor I

Apparently the P4080 Rev 3.0 has the same problem.

0 Kudos
Reply

4,635 Views
andrei_skok
NXP Employee
NXP Employee

Hello,


Sorry, but the information you are requesting is treated as confidential info at this time and requires a signed NDA (Non-Disclosure Agreement). Naturally, we cannot discuss this with you in public anyway, this requires to be handled as a Service Request (SR). How I could create a Service Request?  Be aware that to give you remote support through a SR, we will still need the confirmation of a NXP employee that the NDA is in place. If you want to go this route, the next steps will be: If you have already signed a NDA agreement for this product, please contact the person who assisted you or create a SR and name us a NXP person that can confirm this. If you have not signed an agreement, please contact your local NXP Distributor Salesperson or FAE for assistance. For a listing of our distributors, refer to: http://www.nxp.com/webapp/sps/site/overview.jsp?code=DISTRIBUTORS


Have a great day,
Andrei


-------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-------------------------------------------------------------------------------

0 Kudos
Reply

4,635 Views
renatomancuso
Contributor I

Andrei,

I talked with my department's staff and they were able to find the signed version of the NDA. I am linking it here for your reference: https://drive.google.com/file/d/0B4RGHmADKIQbS0c3Q3BTU3JsWU0/view?usp=sharing

Thanks in advance for your time.

Best,

Renato

0 Kudos
Reply

4,635 Views
renatomancuso
Contributor I

Dear Andrei,

I am attaching the digital copy of the NDA between Freescale and UIUC. It contains the terms and the number of the agreement.

Sue Rhodes (CC'd) is the person on our side who followed the agreement negotiation back in 2010. The agreement suggests that Todd Salter was our contact at Freescale and should be able to confirm that our NDA is in place.

Thanks in advance for your time.

Best regards,

Renato

0 Kudos
Reply

4,635 Views
andrei_skok
NXP Employee
NXP Employee

Thank you for providing signed NDA. Unfortunately P4080DEBUGRM is a confidential document so we can not discuss it in public community. Please create a Service Request (SR)How I could create a Service Request?  starting with "Hello Andrei" and I will do my best to help you.


Have a great day,
Andrei

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

4,635 Views
renatomancuso
Contributor I

Dear Andrei,

I have followed your suggestion and started a new case with my question.

Best regards,

Renato

0 Kudos
Reply