Qustion for BSC9131 in LTE solution

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Qustion for BSC9131 in LTE solution

1,367件の閲覧回数
symsong
Contributor II

     HI,I'm working with bsc9131 and want to get start with the FreeScale LTE solution,is there any related documents that I can refer to and how can I get it?

0 件の賞賛
返信
4 返答(返信)

1,236件の閲覧回数
michelle
NXP Pro Support
NXP Pro Support

Hi

The IPC demos can be found in our WUSDK version 1.6 being the latest).  There should be two of these already built along with DSP side binaries in the /images/ipc directory.

Any LTE demos typically run with both Linux and the DSP side code, however if you are referring to our L2shim which we use for testing purposes.  Some end to end testing uses a purely DSP side approach with the CodeWarrior debugger being used to run TCL scripts to setup test parameters and check results.

0 件の賞賛
返信

1,236件の閲覧回数
r8070z
NXP Employee
NXP Employee

Have a great day,

I suppose that you may start from the BSC9131 page

http://www.nxp.com/products/microcontrollers-and-processors/power-architecture-processors/qoriq-qonv...

and the BSC9131RDB page

http://www.nxp.com/products/power-management/switching-regulator/qoriq-qonverge-bsc9131-rdb-for-femt...

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,236件の閲覧回数
symsong
Contributor II

and also I'm thinking that whether the LTE BaseStation test is controled by U-Boot only,or I should use CodeWarrior to debug it?

0 件の賞賛
返信

1,236件の閲覧回数
symsong
Contributor II

Thanks,and I want to know where can I find the IPC demos which mentioned in the QSG.

0 件の賞賛
返信