Question for LS1021A RCW configuration

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Question for LS1021A RCW configuration

3,076 次查看
yongsheng_he
Contributor I

Hi, Dear NXP Tech Support Team:

I want to confirm the RCW value of the LS1021A  board I am working on when it came out of the factory and noticed that there is an example on page 2 of the doc AN5089, is that just an example or the actual RCW for the LS1021A board? My board has exactly the same RCW value what the example says, but it is not working on our system, the serial output stops after showing 'DRAM: 1 GiB'. 
But the documents show this board was working before when the middle of the last line of the RCW was '281b7340' as what shows in the attached image at the bottom of this question. I do not have the background of this board and do not know if its RCW had been programmed to be '281b7340' after we purchased. 
So the question is which one is the factory default set, '881b7340' or '281b7340' or any other?
CPU: Freescale LayerScape LS1021E, Version: 2.0, (0x87081120)
Clock Configuration:
CPU0(ARMV7):1000 MHz,
Bus:300 MHz, DDR:800 MHz (1600 MT/s data rate),
Reset Configuration Word (RCW):
00000000: 0608000a 00000000 00000000 00000000
00000010: 70000000 00007900 e0025a00 21046000
00000020: 00000000 00000000 00000000 20000000
00000030: 00080000 281b7340 00000000 00000000
Thanks
Kevin
3 回复数

2,794 次查看
yipingwang
NXP TechSupport
NXP TechSupport

Hello Kevin He,

Please refer to the following bit 416-418 in LS1021 RCW configuration, please refer to 010 and 100 options.

416-418 EC1 Selects the functionality
assigned to the EC1 pins:
EC1_TXD3, EC1_TXD2,
EC1_TXD1, EC1_TXD0,
EC1_TX_EN, EC1_GTX_CLK,
EC1_GTX_CLK125,
EC1_RXD3, EC1_RXD2,
EC1_RXD1, EC1_RXD0,
EC1_RX_CLK, EC1_RX_DV
Options:
000 RGMII1
001 GPIO3[2:14]
010 CAN2_TX, CAN1_TX, Reserved, Reserved,
Reserved, Reserved, Reserved, CAN2_RX,
CAN1_RX, Reserved, Reserved, Reserved, Reserved
011 MII1 (Note: EC3 must be 011 for MII support.)

100 SAI1_TX_DATA, SAI2_TX_DATA,
SAI1_TX_SYNC, SAI2_TX_SYNC, SAI1_TX_BCLK,
SAI2_TX_BCLK, EXT_AUDIO_MCLK2,
SAI1_RX_DATA, SAI2_RX_DATA, SAI1_RX_SYNC,
SAI2_RX_SYNC, SAI1_RX_BCLK, SAI2_RX_BCLK
101 FTM1_CH5, FTM1_CH7, FTM1_CH3,
FTM1_CH2, FTM1_FAULT, FTM1_EXTCLK,
Reserved, FTM1_CH4, FTM1_CH6, FTM1_CH1,
FTM1_CH0, FTM1_QD_PHA, FTM1_QD_PHB
110 Reserved
111 Reserved

Please refer to RCW provided in the pre_built image ISO.
rcw/ls1021atwr/RSR_PPS_70$ xxd rcw_1000.bin
00000000: aa55 aa55 01ee 0100 0608 000a 0000 0000  .U.U............
00000010: 0000 0000 0000 0000 7000 0000 0000 7900  ........p.....y.
00000020: e002 5a00 2104 6000 0000 0000 0000 0000  ..Z.!.`.........
00000030: 0000 0000 2000 0000 0008 0000 881b 7340  .... .........s@
00000040: 0000 0000 0000 0000 0957 0200 ffff ffff  .........W......
00000050: 09ee 0200 6010 0000 09ea 085c 0050 2880  ....`......\.P(.
00000060: 0861 0040 83c1 eb81                      .a.@....

ls1021atwr/rcw/ls1021atwr/SSR_PNS_30$ xxd rcw_1000.bin
00000000: aa55 aa55 01ee 0100 0608 000a 0000 0000  .U.U............
00000010: 0000 0000 0000 0000 3000 0000 0000 7900  ........0.....y.
00000020: e002 5a00 2104 6000 0000 0000 0000 0000  ..Z.!.`.........
00000030: 0000 0000 1800 0000 0008 0000 481b 7340  ............H.s@
00000040: 0000 0000 0000 0000 0957 0200 ffff ffff  .........W......
00000050: 09ee 0200 6010 0000 09ea 085c 0050 2880  ....`......\.P(.
00000060: 0861 0040 e7a2 5a83                      [email protected].

In fact, I consider your DDR problem should be caused by the improper DDR controller configuration in u-boot.

If you are bringing up a new target board, you need to customize DDR controller configuration section in u-boot according to your target board.

We often suggest customers create a QCVS project according to DDR datasheet or reading from SPD, then use DDRv tool to do optimization and validation.


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

2,794 次查看
sparekh
Contributor I

What are the first 8 bytes of the RCW?  aa55 aa55 01ee 0100?  After power up, when I read the RCW register inside the processor with a JTAG/COP, I do not see these bytes.  The RCW contains next 56 bytes.  But I can see with a logic analyzer that these 8 bytes are coming out the sd-card.  And the CPU doesn't boot.  

Where should I look?  Any ideas?

Thank you.

Best regards,

Sanjay 

0 项奖励
回复

2,794 次查看
yongsheng_he
Contributor I

Got it, thanks a lot Yiping

Regards

Kevin

On Tue, Sep 18, 2018 at 3:19 AM, Yiping Wang <[email protected]>

0 项奖励
回复