Power Consumption onf LS1012A Development Boards

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Power Consumption onf LS1012A Development Boards

ソリューションへジャンプ
1,864件の閲覧回数
joe1652
Contributor IV

Hello, I am looking for design a board using the LS1012A ARM processor. I am looking at my power requirements and have a question that I hope someone can help me with. According to the documentation on the XFRWY-LS101A-PA Rev-B board the power consumption is 16W at 1A. Is there any information on how much current the board is consuming on the 0.9V, 1.35V, 1.8V and the 2.5V rails? I need this to determine if I will need a heat sink on my input regulator. My input voltage is 18V so I need to find a regulator that won't get too hot.

Thanks,

Joe

1 解決策
1,791件の閲覧回数
ufedor
NXP Employee
NXP Employee

Power consumption of the XFRWY-LS1012A:

Supply [V]Max. Current [A]
3.33.2
1.80.4
1.350.6
0.91.35

2.5V - not used.

元の投稿で解決策を見る

1 返信
1,792件の閲覧回数
ufedor
NXP Employee
NXP Employee

Power consumption of the XFRWY-LS1012A:

Supply [V]Max. Current [A]
3.33.2
1.80.4
1.350.6
0.91.35

2.5V - not used.