P5020 Secure Boot

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

P5020 Secure Boot

6,778 Views
analim_gt
Contributor I

I am attempting to secure boot a P5020 and so far my attempts have not been successful.

I am reading in the SDK documentation, it sounds like a HASH has to be program in the SFP fuse. It also looks like the fuse can only be programed two times. Is there anyway to perform secure boot without programing the fuse?

I am very new to all of this, any help is appreciated.

Tags (2)
0 Kudos
Reply
10 Replies

6,548 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello Ana Lim,

You could set SB_EN bit to 1 in RCW to enable secure boot.

You could write SRK hash keys to the mirror registers in the prototype stage.

For details, please refer to https://community.nxp.com/docs/DOC-332248 

Thanks,

Yiping

0 Kudos
Reply

6,548 Views
analim_gt
Contributor I

Hi Yiping,

Any feedback?

I am trying to also figure out the address of the shadow registers? Any suggestions?

0 Kudos
Reply

6,548 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello Ana Lim,

Please use secure RCW provided in SDK 1.9.

I uploaded QorIQ Linux SDK 2.0 user manual https://drive.google.com/open?id=1-goeJsMtBB1X7X9Bfo9NV42YhAs_iuOM , please refer to the section "10.3.1.14 Appendix P3/P4/P5/T1_T2_T4 Secure Boot demo".

Please refer to the following CCS command for P5020

# Connect to CCS and configure Config Chain
ccs::config_chain p3040
display ccs::get_config_chain
#Check Initial SNVS State and Value in SCRATCH Registers
ccs::display_mem 0 0xfe314014 4 0 1
ccs::display_mem 0 0xfe0e0200 4 0 4
#Wrie the SRK Hash Value in Mirror Registers
ccs::write_mem 0 0xfe0e807c 4 0 <SRKH1>
ccs::write_mem 0 0xfe0e8080 4 0 <SRKH2>
ccs::write_mem 0 0xfe0e8084 4 0 <SRKH3>
ccs::write_mem 0 0xfe0e8088 4 0 <SRKH4>
ccs::write_mem 0 0xfe0e808c 4 0 <SRKH5>
ccs::write_mem 0 0xfe0e8090 4 0 <SRKH6>
ccs::write_mem 0 0xfe0e8094 4 0 <SRKH7>
ccs::write_mem 0 0xfe0e8098 4 0 <SRKH8>
#Get the Core Out of Boot Hold-Off
ccs::write_mem 0 0xfe0e00e4 4 0 0x00000001

Thanks,

Yiping

0 Kudos
Reply

6,548 Views
analim_gt
Contributor I

Hi Yiping,

The ccs commands above only write hash to the SRKH. Do I need to burn the OTPMK since those registers seems to be write protected?

I am seeing the SCRATCHRW2=0x00010000 and SECMON_HPSR=0x812d0b00.

Ana

0 Kudos
Reply

6,548 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello Ana,

You need to burn OTPMK and please make sure bits OTPMK_ZERO, OTMPK_SYNDROME and PE are 0 of the status register of sec mon block.

Thanks,

Yiping

0 Kudos
Reply

6,544 Views
ramakrishna_bik
Contributor I

Where can I find information about these registers for different boards? I am interested in P4080DS and P5040 boards. What is the address and which bits represent them? I am not able to find them in SDK 2.0 documentation and TRM for the boards. Greatly appreciate your help in this regard. Thank you!

0 Kudos
Reply

6,549 Views
analim_gt
Contributor I

Yiping, thanks!

I am seeing a mention of running the OTPMK Hamming algorithm on the OTPMK hash. Is that necessary? 

Can the OTPMK hash be obtained the same way as the SRKHR?

I am suing the provide uni_sign tool to get the SRKHR hash, can it be used for the OTPMK hash? 

Also, is the OTPMK hash need to be byte swapped? From the Setting up Secure boot document, the way that OTPMK hash is listed is a bit different from the SRKHR (which has no mention of bit order).

OTPMK.pngSRKHR.png

0 Kudos
Reply

6,549 Views
yipingwang
NXP TechSupport
NXP TechSupport

Blow OTPMK to fuse array is necessary to enable secure boot.

Generate OTPMK key with CST command gen_otpmk_drbg, please refer to the following.

./gen_otpmk_drbg <bit_order> [string]
<bit_order> : (1 or 2) OTPMK Bit Ordering Scheme in SFP
1 : BSC913x, P1010, P3, P4, P5, C29x
2 : T1, T2, T4, B4, LSx
<string> : 32 byte string

No need to do swapping for the generate OTPMK key.

0 Kudos
Reply

6,549 Views
analim_gt
Contributor I

Thanks Yiping!

0 Kudos
Reply

6,549 Views
analim_gt
Contributor I

Hi Yiping,

Thanks for your answer. I am reviewing the document above and have some questions.

In the document the PBI commands are as follow, but it is a bit different than the rcw that i am using (from SDK 1.9).

Setting up Secure Boot on PBL Based Platforms in Prototype StageRCW from SDK1.9 for p5020
rcw_15g_sben_2000mhz.bin

#LAW for ESBC

09000c10 00000000

09000c14 c0000000

09000c18 81f0001b

# LAW for CPC/SRAM

09000d00 00000000

09000d04 bff00000

09000d08 81000013

# Scratch Registers

090e0200 c0b00000

090e0208 c0c00000

# CPC SRAM

09010100 00000000

09010104 bff00009

# CPC Configuration

09010f00 08000000

09010000 80000000

#LAW for ESBC

09000cd0 00000000
09138000 00000000
09000cd4 c0000000

09138000 00000000
09000cd8 81f0001d

09138000 00000000

# Scratch Registers

090e0200 c0b00000

In the rcw_15g_sben_2000mhz.bin, there is not commands to write the CPC/SRAM. Are they not needed on p5020?

Also, in the "Setting up Secure Boot on PBL Based Platforms in Prototype Stage", there is a section to write the keys hash in ccs. However, the QorIQ P5020 Reference Manual 5.4.2.1, said that those register are blocked during secure boot.

                        blocked registers.png

I did try to write to the 0xe_805c and confirmed that the write did not go successfully.

Did I miss something?

0 Kudos
Reply