P3041DS-PC - Aurora support?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

P3041DS-PC - Aurora support?

1,288件の閲覧回数
miguelgarciacle
Contributor I

For our project we are looking for a Freescale board with VxWorks 7 BSP and Aurora debugging interface.

The P3041DS-PC is the only board that I have found with VxWorks 7 BSP and where in the high-level description it is explicitly mentioned that it has an Aurora connector.

Is it then the standard 70-pin connector? Can I then assume that the Aurora interface is working in that board (software support in the SDK)?

Thanks a lot

Miguel

0 件の賞賛
返信
1 返信

1,217件の閲覧回数
ufedor
NXP Employee
NXP Employee

> Is it then the standard 70-pin connector

Yes, the board is equipped with standard 70-pin Aurora connector and supports Aurora (up to x2 lanes).

> Can I then assume that the Aurora interface is working in that board

Yes.

> (software support in the SDK)?

CodeWarrior supports Aurora.

0 件の賞賛
返信