Hi all,
In my card, based on P2041rdb, i'm using software "Linux-3.8.13-rt9-QorIQ-SDK-V1.4".
Facing below error after some time around 2-3 mins, while running application which is using IPC concepts, like shared memory and semaphore.
sh: error while loading shared libraries: libtinfo.so.5: cannot open shared object file: Error 24
Can anyone pls let me know what is the exact meaning by above error. And how to get this package ??
thanks,
Gourav
We have tested SDK v1.4 using Ubuntu 12 32bit.
The following command sequence was used:
Message: /bin/sh -> dash
Answer after password – No
Message:
Removing 'diversion of /bin/sh to /bin/sh.distrib by dash'
Adding 'diversion of /bin/sh to /bin/sh.distrib by bash'
Removing 'diversion of /usr/share/man/man1/sh.1.gz to /usr/share/man/man1/sh.distrib.1.gz by dash'
Adding 'diversion of /usr/share/man/man1/sh.1.gz to /usr/share/man/man1/sh.distrib.1.gz by bash'
Message: /bin/sh -> bash
Usually Linux recommends also run the following command: sudo usr/sbin/visudo
Have a great day,
Pavel Chubakov
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------