How to run Linux on LS1012A Dev Board(XFRWY-LS1012A-PA)?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to run Linux on LS1012A Dev Board(XFRWY-LS1012A-PA)?

Jump to solution
1,162 Views
joseph_lindula
Contributor IV

Hello, I using the LS1012A Dev Board(XFRWY-LS1012A-PA) to learn how to use the LS1012A on my next hardware design. I will be using Linux on the LS1012A on my next design. In order to learn how to run Linux on the LS1012A I thought it would be learning experiment to load Linux on the LS1012A Dev board. How is this done?

Do I need to put Linux on a SD card like what it is done on the BeagleBone Black board? Or, can I use CodeWarrior to load Linux? Can I load Linux on the SPI flash and boot Linux from that memory?  I would prefer not to have to use an SD card to load Linux.

Thank you very much,

Joe

1 Solution
1,030 Views
Pavel
NXP Employee
NXP Employee

The LS1012a supports booting only from QSPI NOR Flash. See the Section 24.1 of the LS1012a Reference Manual:

https://www.nxp.com/webapp/Download?colCode=LS1012ARM

 

See the Chapter 4.1.1 of the LSDK 18.12 documentation about LSDK using for the FRWY-LS1012A board:

https://www.nxp.com/docs/en/supporting-information/LSDK-KC-REV18.12.pdf

 

See also the Section 4.1.1.4 about deploying LSDK images on the board.

 

The Section 8.6.3 in the ARMv8_Targeting_Manual.pdf file contains information about program U-Boot in flash device using Flash Programmer.

This file is available in CW4NET folder.


Have a great day,
Pavel Chubakov

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

3 Replies
1,030 Views
Pavel
NXP Employee
NXP Employee

Load and install evaluation version of CodeWarrior CW4NET using the following page:

https://www.nxp.com/support/developer-resources/software-development-tools/codewarrior-development-t...


Have a great day,
Pavel Chubakov

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

1,031 Views
Pavel
NXP Employee
NXP Employee

The LS1012a supports booting only from QSPI NOR Flash. See the Section 24.1 of the LS1012a Reference Manual:

https://www.nxp.com/webapp/Download?colCode=LS1012ARM

 

See the Chapter 4.1.1 of the LSDK 18.12 documentation about LSDK using for the FRWY-LS1012A board:

https://www.nxp.com/docs/en/supporting-information/LSDK-KC-REV18.12.pdf

 

See also the Section 4.1.1.4 about deploying LSDK images on the board.

 

The Section 8.6.3 in the ARMv8_Targeting_Manual.pdf file contains information about program U-Boot in flash device using Flash Programmer.

This file is available in CW4NET folder.


Have a great day,
Pavel Chubakov

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

1,030 Views
joseph_lindula
Contributor IV

The file, " ARMv8_Targeting_Manual.pdf" is that found in the Code Warrior directory? I don't have Code Warrior installed, is that a free download?

0 Kudos
Reply