P2020 eTSEC clocks needed for SGMII connection

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

P2020 eTSEC clocks needed for SGMII connection

1,549 次查看
dank4
Contributor II

i want to connect the P2020 eTSEC to an SGMII interfaced phy (88e1512) , 

which clocks should i be connecting at the P2020 , 

these i am sure of :

  • P2020 sys clock  - V
  • P2020 serdes lanes - sd ref clk - V

but about this one :

  • do i need to clock the eTSEC clock input as well - ? 

Thanks ahead 

标记 (2)
0 项奖励
回复
1 回复

1,442 次查看
ufedor
NXP Employee
NXP Employee

> do i need to clock the eTSEC clock input as well - ?

No - refer to the P2020 QorIQ Integrated Processor Reference Manual, Table 14-1. eTSECn network interface signal properties:

"EC _GTX_CLK125

Oscillator source for GMII, TBI, RGMII, RTBI transmit clock, input, shared by all eTSECs"