P1024/p1015

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

P1024/p1015

945 次查看
rajeshpuppala
Contributor I

UBOOT for p1024/p1015

0 项奖励
回复
2 回复数

601 次查看
Pavel
NXP Employee
NXP Employee

NXP SDK 1.3 and 1.3.2 support P1024/P1015. See SDK documentation. 

NXP SDK 1.3 and 1.3.2 are available on NXP page. Use SDKLINUX for search. Download previous version of NXP SDK.

Use iso image for e500v2 core. This image contains u-boot binary image


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

601 次查看
ufedor
NXP Employee
NXP Employee

The U-Boot sources are provided in the NXP Linux SDK v1.9 freely available at:

https://nxp.flexnetoperations.com/control/frse/download?agree=Accept&element=7126427 

0 项奖励
回复