P1024/p1015

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

P1024/p1015

874 Views
rajeshpuppala
Contributor I

UBOOT for p1024/p1015

0 Kudos
Reply
2 Replies

530 Views
Pavel
NXP Employee
NXP Employee

NXP SDK 1.3 and 1.3.2 support P1024/P1015. See SDK documentation. 

NXP SDK 1.3 and 1.3.2 are available on NXP page. Use SDKLINUX for search. Download previous version of NXP SDK.

Use iso image for e500v2 core. This image contains u-boot binary image


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

530 Views
ufedor
NXP Employee
NXP Employee

The U-Boot sources are provided in the NXP Linux SDK v1.9 freely available at:

https://nxp.flexnetoperations.com/control/frse/download?agree=Accept&element=7126427 

0 Kudos
Reply