P1024/p1015

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

P1024/p1015

947件の閲覧回数
rajeshpuppala
Contributor I

UBOOT for p1024/p1015

0 件の賞賛
返信
2 返答(返信)

603件の閲覧回数
Pavel
NXP Employee
NXP Employee

NXP SDK 1.3 and 1.3.2 support P1024/P1015. See SDK documentation. 

NXP SDK 1.3 and 1.3.2 are available on NXP page. Use SDKLINUX for search. Download previous version of NXP SDK.

Use iso image for e500v2 core. This image contains u-boot binary image


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

603件の閲覧回数
ufedor
NXP Employee
NXP Employee

The U-Boot sources are provided in the NXP Linux SDK v1.9 freely available at:

https://nxp.flexnetoperations.com/control/frse/download?agree=Accept&element=7126427 

0 件の賞賛
返信