P1010 platform kexec feature support

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

P1010 platform kexec feature support

3,480 Views
qingshanli
Contributor I

hi

I am use p1010 cpu and SDK version is 1.5. Now i test kexec feature on this platform with below command:

kexec --load --initrd=/tmp/initrd --

append="console=ttyS0,115200" /tmp/kernel

umount -ar

kexec --exec

after commands execute finish, the console just print info:

Starting new kernel

Bye!

and then the cpu system looks like freeze,and console don't

have any information output.

I further debug source code and found "kexec --exec" final call

function default_machine_kexec

(arch/powerpc/kernel/machine_kexec_32.c)

, execute below codes

....

/* now call it */

62 rnk = (relocate_new_kernel_t) reboot_code_buffer;

63 (*rnk)(page_list, reboot_code_buffer_phys, image-

>start);

and then cpu looks like freeze.

I don't know how to debug it and please help confirm it

whether this situation is SDK bug.

P.S

/tmp/initrd is initrd file

/tmp/kernel is elf vmlinux file

in uboot mode i can use initrd and kernre file can bootup cpu

system, so the two file is correct.

0 Kudos
Reply
6 Replies

3,297 Views
scottwood
NXP Employee
NXP Employee

While there is some code present for kexec, it's not currently a supported/tested feature of the SDK.  If you need support for this, let your sales/FAE contact know.

0 Kudos
Reply

3,297 Views
qingshanli
Contributor I

hi scott

your reply mention "some codes present for kexec", whether you can offer those codes to me so i can test kexec feature on p1010 platform?

0 Kudos
Reply

3,297 Views
scottwood
NXP Employee
NXP Employee

I'm referring to the code that is already in the kernel.  What I'm saying is that somebody worked on it in the past, but I don't think it is currently expected to work.

0 Kudos
Reply

3,298 Views
qingshanli
Contributor I

hi Scott

I test kexec feature on 3.9.6 Kernel and found it works. But 3.9.6 kernel is not my favorite kernel version. I can merge some codes form 3.9.6 to 3.8.13 for 3.8.13 can support kexec feature but i don't know how to start it. Whether you can help me to achieve it?

0 Kudos
Reply

3,298 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello Qingshan,

Please also provide Kernel configuration files for both original Kernel and dump capture Kernel.

Thanks,

Yiping

0 Kudos
Reply

3,294 Views
qingshanli
Contributor I

hi yiping

both kernel use the same config file

0 Kudos
Reply