Need help with package manager b4860

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Need help with package manager b4860

1,098 次查看
chandramills
Contributor I

I eventually want to install GNU Radio on the PPC64 board (b4860).  I have tried adding meta-sdr to the yocto build.  The build fails.  Is there some support for:

1. How to include a package manager to the fsl-image-full build

2. How to add the gnu radio package to either the fsl-image-full build or install gnu radio packages from another source directly to the board?

3. HOw to flash a fsl-image-full build to the b4860?

Thanks,

C-

0 项奖励
回复
1 回复

1,022 次查看
Pavel
NXP Employee
NXP Employee

Look at the following page

https://freescale.sdlproducts.com/LiveContent/web/pub.xql?action=home&pub=LS2085A%20EAR%20v5.0%20-%2...

It is FAQ for NXP SDK. Find the following on this page:

How do I install the source code, modify it, and then and rebuild u-boot/kernel?


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复