Manual for P2041RDB-PC ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Manual for P2041RDB-PC ?

2,209 Views
clarktucker
Contributor I

I can't seem to locate the documentation that came with my P2041RDB-PC platform.  Searching the NXP site and elsewhere only turns up a sparse 'fact sheet'.  Specifically, I'm looking for the DIP switch definitions and information about the boot process.  I'd love a link to the guide/reference manual for the platform, but any related information would be helpful.  Thanks!

--clark

0 Kudos
Reply
3 Replies

2,084 Views
clarktucker
Contributor I

Thanks for the pointer, the SDK documentation does provide a little insight into the switches, but I think I still need a reference manual for the board.

Concerning requesting the manual from the manufacturer:  I thought NXP (Freescale) was the manufacturer... Is there a better channel to make the request?

Thanks again!

0 Kudos
Reply

2,084 Views
r8070z
NXP Employee
NXP Employee

It is supposed that vendor supplies board and its documentation. If for some reason there is not manual on the nxp site then it cannot be published on nxp community pages too. To obtain the manual please create a Technical Case as shown on https://community.freescale.com/thread/381898

0 Kudos
Reply

2,084 Views
r8070z
NXP Employee
NXP Employee


Have a great day,

You can request the manual from the board vendor. Default switch settings and some switches info of the P2041RDB you can get from QorIQ SDK v2.0-1703 Documentation available on webpage

https://www.nxp.com/support/developer-resources/run-time-software/linux-software-and-development-too...

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply