Low disk space

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Low disk space

1,906件の閲覧回数
aravindganesan
Contributor I

Hello

I have installed QorIQ SDK V1.6 in Ubuntu 12.04.

I have also setuo the host environment.

Now I have to install RapidIO driver.

But I am getting a warning saying:""""Low disk space:::Only 300 bytes of space remaining""""""

I am running Ubuntu as a dual-OS along with Windows7.

Though I am not having enough space in my /home partition(that is where the SDK1.6 is installed) i am having 200GB space as an external volume(mounted separately).

So can i just copy the QorIQ folder installed in my /home to my external volume and continue my further installations?

Or should I repeat the entire process again by creating more space in /home for which i will have to reinstall Ubuntu.

Please advise.

タグ(3)
0 件の賞賛
返信
2 返答(返信)

1,764件の閲覧回数
sam_lee
Contributor II

yes,I think you can copy the SDK to other storage location and creat a soft link to the SDK in the old installed directory. I did it before and it works.

hopes it help.

Regards

Sam

1,764件の閲覧回数
aravindganesan
Contributor I

Dear Sam Lee,

Thanks for your clue.

I will try.

Aravind

0 件の賞賛
返信