LS1046ARDB development board MINIPCIE interface used network card model?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LS1046ARDB development board MINIPCIE interface used network card model?

1,196 次查看
17319399281
Contributor I

We are using the LS1046A development board. We want to use the MINIPCIE interface above to realize wifi and bluetooth functions. Is there any recommended model

When the development board is designed, when the wifi function is tested, which interface is used?What type of network card.

The module needs to integrate both wifi and bluetooth functions. Wifi supports AP mode and bluetooth V4.2 or above

0 项奖励
回复
1 回复

1,120 次查看
ufedor
NXP Employee
NXP Employee

The WNC DNXA-H1 was tested with the LS1046ARDB - please refer to:

https://www.nxp.com/docs/en/user-guide/IIoT_UG.pdf 

0 项奖励
回复