LS1046ARDB development board MINIPCIE interface used network card model?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LS1046ARDB development board MINIPCIE interface used network card model?

1,211件の閲覧回数
17319399281
Contributor I

We are using the LS1046A development board. We want to use the MINIPCIE interface above to realize wifi and bluetooth functions. Is there any recommended model

When the development board is designed, when the wifi function is tested, which interface is used?What type of network card.

The module needs to integrate both wifi and bluetooth functions. Wifi supports AP mode and bluetooth V4.2 or above

0 件の賞賛
返信
1 返信

1,135件の閲覧回数
ufedor
NXP Employee
NXP Employee

The WNC DNXA-H1 was tested with the LS1046ARDB - please refer to:

https://www.nxp.com/docs/en/user-guide/IIoT_UG.pdf 

0 件の賞賛
返信