LS1046A ethernet link down/up problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1046A ethernet link down/up problem

2,327 Views
Gyosun
Contributor III

Hello,

 

I am using an LS1046A custom board using SDK-1703 version.

I am using AR8035-AL1B 1G phy connected to fm1-mac3 via RGMII interface.

If you link down/up after about 30 minutes after booting, you will see a phenomenon that the up will not work.

It seems that the initialization is not working properly. Is there a solution?

 

------------------------- test -----------------------------------

root@ls1046ardb:~# uptime

10:59:59 up 33 min,  1 user,  load average: 0.00, 0.00, 0.00

root@ls1046ardb:~# ifconfig fm1-mac3 down

root@ls1046ardb:~# ifconfig fm1-mac3 up

SIOCSIFFLAGS: No such device

… dmesg …

[ 1992.532681] fsl_dpa fsl,dpaa:ethernet@2 fm1-mac3: Could not connect to PHY /soc/fman@1a00000/mdio@fc000/ethernet-phy@1

[ 1992.532687] fsl_dpa fsl,dpaa:ethernet@2 fm1-mac3: init_phy() = -19

…

 

Thank you!

Best Regards,

Gyosun.

0 Kudos
Reply
3 Replies

2,312 Views
yipingwang
NXP TechSupport
NXP TechSupport

Linux Kernel provided in SDK 2.0 1703 doesn't include AR8035 PHY driver.

Please refer to PHY AR8035 driver patch provided in http://linux-kernel.2935.n7.nabble.com/PATCH-net-phy-Add-Atheros-AR8035-PHY-support-td637283.html

 Please enable ATHEROS_PHY in Linux Kernel.

In addition, would you please provide the result of command "mdio list" in u-boot?

Would you please also send your dts file to me to do more investigation.

0 Kudos
Reply

2,308 Views
Gyosun
Contributor III

Hi yipingwang,

Thank you for answer.

The point of the question seems to have not been communicated well.

We have connected the AR8035 and are using it well.

If you don't just do the link down command, ethernet works without problems.

However, if you link down and up after about 30 minutes, it does not come back.

This is the result of mdio list.

=> mdio list
FSL_MDIO0:
0 - AR8035 <--> FM1@DTSEC6
FM_TGEC_MDIO:

 

Attach the kernel net folder source code and dts & config files.

analysis_210325.zip 

 

Could you please review why the link doesn't come back to life?

 

Thank you!

Best Regards,

Gyosun.

 

0 Kudos
Reply

2,298 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello Gyosun,

In your Kernel source code, I didn't find PHY driver for AR8035, please apply the following patch to your Linux Kernel and enable ATHEROS_PHY in Kernel configuration file.

http://linux-kernel.2935.n7.nabble.com/PATCH-net-phy-Add-Atheros-AR8035-PHY-support-td637283.html

 

Thanks,

Yiping

0 Kudos
Reply