LS1046A emmc

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1046A emmc

4,603 Views
anle
Contributor I

      I use SK hynix H26M51002KPR instead of H26M52208FPR,when I download Uboot imange to emmc,can“t find;Data bus width : 4bits;

also I change it to 8bits,No change;

      I'll have to find cause,So,I need help to find it ,please!

0 Kudos
Reply
3 Replies

4,430 Views
Pavel
NXP Employee
NXP Employee

Check the LS1043a RCW SPI_BASE and SPI_EXT fields.

It looks like there is a hardware problem on your board.

This eMMC is not detected on your board.

Check connection and power supply of this eMMC.

Have a great day,
Pavel Chubakov

0 Kudos
Reply

4,430 Views
Pavel
NXP Employee
NXP Employee

Is there possibility to boot from QSPI/NOR/NAND?

Boot from QSPI/NOR/NAND and test reading writing your eMMC.

Have a great day,
Pavel Chubakov

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

4,430 Views
anle
Contributor I

Hi,Pavel ;

   I'm so sorry for replying to you late ,I had a  holiday last weekend. My board  boot form QSPI flash ,Reading eMMC information through command "mmc info” in u-boot ,

   I had uploaded the log file, FYI,Thanks.

log.jpg

0 Kudos
Reply