LS1043ARDB does it support ebtables

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LS1043ARDB does it support ebtables

ソリューションへジャンプ
1,701件の閲覧回数
abhijeet_sasmal
Contributor I

Does it support ebtables?

0 件の賞賛
返信
1 解決策
1,641件の閲覧回数
bpe
NXP Employee
NXP Employee

ebtables is a generic Linux tool, we support it as long as the kernel
does. If the question is about hardware acceleration, the answer is
no, there is another tool that controls packet filtering, header manipulation
and automatic forwarding at the DPAA level, called FMC. Details can be
found here


Have a great day,
Platon

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,642件の閲覧回数
bpe
NXP Employee
NXP Employee

ebtables is a generic Linux tool, we support it as long as the kernel
does. If the question is about hardware acceleration, the answer is
no, there is another tool that controls packet filtering, header manipulation
and automatic forwarding at the DPAA level, called FMC. Details can be
found here


Have a great day,
Platon

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信