LS1043A, PCIe LANE query

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LS1043A, PCIe LANE query

1,115 次查看
logeshs
Contributor II

Hi,

We are using LS1043A, PCIe Gen 2 interface is connected to Trident 2+ broadcom swithc. In LS1043A, Serdes configured as per below configuration of RCW[SRDS_PRTCL_S1] 

For PCIe, Gen 2 we will be configuring either RCW[SRDS_PRTCL_S1] as 1460 or 2460 (i.e, Lane C and lane D is configured as PCIe, Gen2?

In the above said mode kindly confirm me Which SERDES lane will be PCIe lane 0 and PCIe lane 1?

Please confirm shall i consider Lane C of LS1043A as lane 0 of trident 2+ and Lane D of LS1043A as lane 1 of Trident 2+?

Thanks

0 项奖励
回复
1 回复

962 次查看
r8070z
NXP Employee
NXP Employee

Have a great day,

Consider Lane C as lane 0, Lane D as lane 1

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复