LS1043A OpenWrt Building UBOOT Flash Image

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LS1043A OpenWrt Building UBOOT Flash Image

8,265 次查看
tmorrison
Contributor III

Hi,

I have a LS1043a-rgw/rdb custom board, and I am using OpenWrt 19.07 and trying to build both

a  NAND and SD Card images.

It is using the LSDK 19.03 u-boot image, but I am finding that the only thing that it does make

are TFA based images - which is NOT what I want.

How can I build Non-Secure/Non-TFA NAND & SD Card images

Tom

0 项奖励
回复
9 回复数

7,964 次查看
yipingwang
NXP TechSupport
NXP TechSupport

Hello Tom,

I just discussed with the development team, it is difficult to build Non-TFA u-boot in OpenWrt automatically.

You could build SD/NAND u-boot image manually.

You could download ARM64 toolchain from the following link

https://drive.google.com/open?id=1DKSXd775Beijes9eMguPfOroAxSWrF6G 

Install toolchain with the following procedure.

$ chmod 777 fsl-qoriq-glibc-x86_64-fsl-toolchain-aarch64-toolchain-3.0.sh

$./fsl-qoriq-glibc-x86_64-fsl-toolchain-aarch64-toolchain-3.0.sh

$ source environment-setup-aarch64-fsl-linux

Please go to folder build_dir/target-aarch64_generic_musl/uboot-layerscape-ls1043ardb/uboot-layerscape-lsdk-1903, build u-boot with the following command.

$make  ls1043ardb_nand_defconfig (for SD u-boot $make ls1043ardb_sdcard_defconfig)

$make CROSS_COMPILE=aarch64-fsl-linux-

Thanks,

Yiping

0 项奖励
回复

7,964 次查看
tmorrison
Contributor III

The toolchain is built into the staging directory...I will try this and see what happens!

t

0 项奖励
回复

7,965 次查看
tmorrison
Contributor III

It builds almost to the end - but it doesn't know how to build spl (fails the mkimage command)...

(without a lot of failure information).

I think all I need to do is correctly create the full uboot (nand and sdcard) that includes:

  • rcw
  • spl (uboot)
  • uboot/environment...
  • fman uCode
  • qe uCode

?

0 项奖励
回复

7,965 次查看
yipingwang
NXP TechSupport
NXP TechSupport

I have verified the above procedure, u-boot-with-spl-pbl.bin has been generated.

0 项奖励
回复

7,965 次查看
tmorrison
Contributor III

Yes, I also got it to work (it was a typo) last night

Does your team have any suggestions on the layout recipe - this seems to

be different than the the layout we have been using manually:

  • IMAGE/sdcard.img := \ ls-clean | \ ls-append-sdhead $(1) |

pad-to 4K | \ ls-append $(1)-uboot.bin | pad-to 3M | \ ls-append

$(1)-uboot-env.bin | pad-to 9M | \ ls-append ls1043ardb-fman.bin |

pad-to 15M | \ ls-append-dtb $$(DEVICE_DTS) | pad-to 16M | \

append-kernel | pad-to $(LS_SD_ROOTFSPART_OFFSET)M | \ append-rootfs |

check-size $(LS_SD_IMAGE_SIZE)*

0 项奖励
回复

7,964 次查看
yipingwang
NXP TechSupport
NXP TechSupport

Please refer to LS1043ARDB memory map provided in target/linux/layerscape/image/armv8_64b.mk.

define Device/ls1043ardb-sdboot
DEVICE_TITLE := LS1043ARDB (SD Card Boot)
DEVICE_PACKAGES += \
layerscape-fman-ls1043ardb \
tfa-ls1043ardb-sdboot \
fmc fmc-eth-config
DEVICE_DTS := freescale/fsl-ls1043a-rdb-sdk
FILESYSTEMS := ext4
IMAGES := sdcard.img
IMAGE/sdcard.img := \
ls-clean | \
ls-append-sdhead $(1) | pad-to 4K | \
ls-append $(1)-bl2.pbl | pad-to 1M | \
ls-append $(1)-fip.bin | pad-to 5M | \
ls-append $(1)-uboot-env.bin | pad-to 9M | \
ls-append ls1043ardb-fman.bin | pad-to 15M | \
ls-append-dtb $$(DEVICE_DTS) | pad-to 16M | \
append-kernel | pad-to $(LS_SD_ROOTFSPART_OFFSET)M | \
append-rootfs | check-size $(LS_SD_IMAGE_SIZE)
endef

0 项奖励
回复

7,964 次查看
tmorrison
Contributor III

Hi Yiping,

Thank you - yes this is what I am trying to customize,

but the map for TFA is different than that of a single

spl & uboot binary.

tom

0 项奖励
回复

7,964 次查看
yipingwang
NXP TechSupport
NXP TechSupport

You could modify

ls-append $(1)-bl2.pbl | pad-to 1M | \
ls-append $(1)-fip.bin | pad-to 5M | \

=>

ls-append $(1)-rcw | pad-to 1M | \
ls-append $(1)-u-boot | pad-to 5M | \

0 项奖励
回复

7,964 次查看
yipingwang
NXP TechSupport
NXP TechSupport

Please refer to the following memory layout

pastedImage_2.png

0 项奖励
回复