LS1043A, IFC Routing Guidelines

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LS1043A, IFC Routing Guidelines

1,834 次查看
logeshs
Contributor II

Hi,

Kindly request you to provide me the LS1043A, IFC interface routing guidelines

Thanks.

0 项奖励
回复
2 回复数

1,667 次查看
alexander_yakov
NXP Employee
NXP Employee

The IFC interface is not very high-speed interface, 100 Mhz max, so there is no specific board layout recommendations.

The only general recommendations could be given:

1. Match signal length for data and control signals for easy understanding of signal timings at remote side

2. Route all signals on the same layer - for same reason, to make signal propagation time to be the same.

3. Use impedance matching techniques to reduce signal ringing on long traces, minimize stubs.


Have a great day,
Alexander

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,667 次查看
logeshs
Contributor II

Hi,

Thanks for your reply.

Do we have any maximum length requirement. If we are matching the length, upto how much mils we can provide tolerance in length matching?

Are there any other precautions to be taken?

Thanks.

0 项奖励
回复