LS1043 Booting Problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1043 Booting Problem

1,738 Views
jayaram
Contributor I

Hi All,

             We are trying to LS1043 based board with kernel 4.1 , but  it is not able to boot. please find the kernel logs below. Can you please help me to resolve this problem.

Starting kernel ...

Booting Linux on physical CPU 0x0
Initializing cgroup subsys cpu
Linux version 4.1.8-rt8 (rajeshwari@rajeshwari) (gcc version 4.9.3 20150311 (prerelease) (Linaro GCC 4.9-2015.03) ) #26 SMP Tue Jan 30 10:51:31 IS
T 2018
CPU: AArch64 Processor [410fd034] revision 4
Detected VIPT I-cache on CPU0
alternatives: enabling workaround for ARM erratum 845719
earlycon: Early serial console at MMIO 0x21c0500 (options '')
bootconsole [uart0] enabled
efi: Getting EFI parameters from FDT:
efi: UEFI not found.
cma: Reserved 16 MiB at 0x00000000bb000000
On node 0 totalpages: 261632
DMA zone: 4088 pages used for memmap
DMA zone: 0 pages reserved
DMA zone: 261632 pages, LIFO batch:31
PERCPU: Embedded 16 pages/cpu @ffffffc03fd90000 s28096 r8192 d29248 u65536
pcpu-alloc: s28096 r8192 d29248 u65536 alloc=16*4096
pcpu-alloc: [0] 0 [0] 1 [0] 2 [0] 3
Built 1 zonelists in Zone order, mobility grouping on. Total pages: 257544
Kernel command line: console=ttyS0,115200 root=/dev/ram0 ramdisk_size=0x10000 earlycon=uart8250,mmio,0x21c0500 maxcpus=1 loglevel=8
log_buf_len individual max cpu contribution: 4096 bytes
log_buf_len total cpu_extra contributions: 12288 bytes
log_buf_len min size: 16384 bytes
log_buf_len: 32768 bytes
early log buf free: 14812(90%)
PID hash table entries: 4096 (order: 3, 32768 bytes)
Dentry cache hash table entries: 131072 (order: 8, 1048576 bytes)
Inode-cache hash table entries: 65536 (order: 7, 524288 bytes)
software IO TLB [mem 0xb6200000-0xba200000] (64MB) mapped at [ffffffc036200000-ffffffc03a1fffff]
Memory: 866520K/1046528K available (5389K kernel code, 445K rwdata, 2188K rodata, 424K init, 203K bss, 163624K reserved, 16384K cma-reserved)
Virtual kernel memory layout:
vmalloc : 0xffffff8000000000 - 0xffffffbdbfff0000 ( 246 GB)
vmemmap : 0xffffffbdc0000000 - 0xffffffbfc0000000 ( 8 GB maximum)
0xffffffbdc2000000 - 0xffffffbdc2ff8000 ( 15 MB actual)
fixed : 0xffffffbffabfd000 - 0xffffffbffac00000 ( 12 KB)
PCI I/O : 0xffffffbffae00000 - 0xffffffbffbe00000 ( 16 MB)
modules : 0xffffffbffc000000 - 0xffffffc000000000 ( 64 MB)
memory : 0xffffffc000000000 - 0xffffffc03fe00000 ( 1022 MB)
.init : 0xffffffc0007e9000 - 0xffffffc000853000 ( 424 KB)
.text : 0xffffffc000080000 - 0xffffffc0007e8504 ( 7586 KB)
.data : 0xffffffc000859000 - 0xffffffc0008c8600 ( 446 KB)
SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=4, Nodes=1
Hierarchical RCU implementation.
Additional per-CPU info printed with stalls.
RCU restricting CPUs from NR_CPUS=64 to nr_cpu_ids=4.
RCU: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=4
NR_IRQS:64 nr_irqs:64 0
GIC CPU mask not found - kernel will fail to boot.
GIC CPU mask not found - kernel will fail to boot.
Architected cp15 timer(s) running at 25.00MHz (phys).
clocksource arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x5c40939b5, max_idle_ns: 440795202646 ns
sched_clock: 56 bits at 25MHz, resolution 40ns, wraps every 4398046511100ns
Console: colour dummy device 80x25
Calibrating delay loop (skipped), value calculated using timer frequency.. 50.00 BogoMIPS (lpj=250000)
pid_max: default: 32768 minimum: 301
Security Framework initialized
Mount-cache hash table entries: 2048 (order: 2, 16384 bytes)
Mountpoint-cache hash table entries: 2048 (order: 2, 16384 bytes)
Initializing cgroup subsys memory
Initializing cgroup subsys hugetlb
hw perfevents: enabled with arm/armv8-pmuv3 PMU driver, 7 counters available
EFI services will not be available.
Brought up 1 CPUs
SMP: Total of 1 processors activated.
CPU: All CPU(s) started at EL2
alternatives: patching kernel code
devtmpfs: initialized
DMI not present or invalid.
clocksource jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns
pinctrl core: initialized pinctrl subsystem
NET: Registered protocol family 16
cpuidle: using governor ladder
cpuidle: using governor menu
vdso: 2 pages (1 code @ ffffffc000861000, 1 data @ ffffffc000860000)
hw-breakpoint: found 6 breakpoint and 4 watchpoint registers.
DMA: preallocated 256 KiB pool for atomic allocations
Serial: AMBA PL011 UART driver
vgaarb: loaded
SCSI subsystem initialized
libata version 3.00 loaded.
usbcore: registered new interface driver usbfs
usbcore: registered new interface driver hub
usbcore: registered new device driver usb
Switched to clocksource arch_sys_counter
NET: Registered protocol family 2
TCP established hash table entries: 8192 (order: 4, 65536 bytes)
TCP bind hash table entries: 8192 (order: 5, 131072 bytes)
TCP: Hash tables configured (established 8192 bind 8192)
UDP hash table entries: 512 (order: 2, 16384 bytes)
UDP-Lite hash table entries: 512 (order: 2, 16384 bytes)
NET: Registered protocol family 1
RPC: Registered named UNIX socket transport module.
RPC: Registered udp transport module.
RPC: Registered tcp transport module.
RPC: Registered tcp NFSv4.1 backchannel transport module.
PCI: CLS 0 bytes, default 64
Trying to unpack rootfs image as initramfs...
rootfs image is not initramfs (no cpio magic); looks like an initrd
in free_reserved_area
Freeing initrd memory: 13116K (ffffffc002e1b000 - ffffffc003aea000)
kvm [1]: interrupt-controller@1404000 IRQ9
kvm [1]: timer IRQ3
kvm [1]: Hyp mode initialized successfully
futex hash table entries: 1024 (order: 4, 65536 bytes)
audit: initializing netlink subsys (disabled)
audit: type=2000 audit(0.000:1): initialized
HugeTLB registered 2 MB page size, pre-allocated 0 pages
VFS: Disk quotas dquot_6.6.0
VFS: Dquot-cache hash table entries: 512 (order 0, 4096 bytes)
NFS: Registering the id_resolver key type
Key type id_resolver registered
Key type id_legacy registered
fuse init (API version 7.23)
9p: Installing v9fs 9p2000 file system support
io scheduler noop registered
io scheduler cfq registered (default)
PCI host bridge /soc/pcie@3500000 ranges:
IO 0x4800010000..0x480001ffff -> 0x00000000
MEM 0x4840000000..0x487fffffff -> 0x40000000
layerscape-pcie 3500000.pcie: PCI host bridge to bus 0000:00
pci_bus 0000:00: root bus resource [bus 00-ff]
pci_bus 0000:00: root bus resource [io 0x0000-0xffff]
pci_bus 0000:00: root bus resource [mem 0x4840000000-0x487fffffff] (bus address [0x40000000-0x7fffffff])
pci 0000:00:00.0: [1957:8080] type 01 class 0x060400
pci 0000:00:00.0: reg 0x10: [mem 0x00000000-0x00ffffff]
pci 0000:00:00.0: reg 0x14: [mem 0x00000000-0x03ffffff]
pci 0000:00:00.0: reg 0x38: [mem 0x00000000-0x00ffffff pref]
pci 0000:00:00.0: supports D1 D2
pci 0000:00:00.0: PME# supported from D0 D1 D2 D3hot
pci 0000:00:00.0: bridge configuration invalid ([bus 00-00]), reconfiguring
pci_bus 0000:01: busn_res: [bus 01-ff] end is updated to 01
pci 0000:00:00.0: BAR 1: assigned [mem 0x4840000000-0x4843ffffff]
pci 0000:00:00.0: BAR 0: assigned [mem 0x4844000000-0x4844ffffff]
pci 0000:00:00.0: BAR 6: assigned [mem 0x4845000000-0x4845ffffff pref]
pci 0000:00:00.0: PCI bridge to [bus 01]
pcieport 0000:00:00.0: enabling device (0000 -> 0002)
pcieport 0000:00:00.0: Signaling PME through PCIe PME interrupt
pcie_pme 0000:00:00.0:pcie01: service driver pcie_pme loaded
aer 0000:00:00.0:pcie02: service driver aer loaded
PCI host bridge /soc/pcie@3600000 ranges:
IO 0x5000010000..0x500001ffff -> 0x00000000
MEM 0x5040000000..0x507fffffff -> 0x40000000
layerscape-pcie 3600000.pcie: PCI host bridge to bus 0001:00
pci_bus 0001:00: root bus resource [bus 00-ff]
pci_bus 0001:00: root bus resource [io 0x10000-0x1ffff] (bus address [0x0000-0xffff])
pci_bus 0001:00: root bus resource [mem 0x5040000000-0x507fffffff] (bus address [0x40000000-0x7fffffff])
pci 0001:00:00.0: [1957:8080] type 01 class 0x060400
pci 0001:00:00.0: reg 0x10: [mem 0x00000000-0x00ffffff]
pci 0001:00:00.0: reg 0x14: [mem 0x00000000-0x03ffffff]
pci 0001:00:00.0: reg 0x38: [mem 0x00000000-0x00ffffff pref]
pci 0001:00:00.0: supports D1 D2
pci 0001:00:00.0: PME# supported from D0 D1 D2 D3hot
pci 0001:00:00.0: bridge configuration invalid ([bus 00-00]), reconfiguring
pci_bus 0001:01: busn_res: [bus 01-ff] end is updated to 01
pci 0001:00:00.0: BAR 1: assigned [mem 0x5040000000-0x5043ffffff]
pci 0001:00:00.0: BAR 0: assigned [mem 0x5044000000-0x5044ffffff]
pci 0001:00:00.0: BAR 6: assigned [mem 0x5045000000-0x5045ffffff pref]
pci 0001:00:00.0: PCI bridge to [bus 01]
pcieport 0001:00:00.0: enabling device (0000 -> 0002)
pcieport 0001:00:00.0: Signaling PME through PCIe PME interrupt
pcie_pme 0001:00:00.0:pcie01: service driver pcie_pme loaded
aer 0001:00:00.0:pcie02: service driver aer loaded
Serial: 8250/16550 driver, 4 ports, IRQ sharing disabled
msm_serial: driver initialized
console [ttyS0] disabled
21c0500.serial: ttyS0 at MMIO 0x21c0500 (irq = 18, base_baud = 18750000) is a 16550A
console [ttyS0] enabled
console [ttyS0] enabled
bootconsole [uart0] disabled
bootconsole [uart0] disabled
21c0600.serial: ttyS1 at MMIO 0x21c0600 (irq = 18, base_baud = 18750000) is a 16550A
21d0500.serial: ttyS2 at MMIO 0x21d0500 (irq = 19, base_baud = 18750000) is a 16550A
21d0600.serial: ttyS3 at MMIO 0x21d0600 (irq = 19, base_baud = 18750000) is a 16550A
Unable to detect cache hierarcy from DT for CPU 0
brd: module loaded
loop: module loaded
tun: Universal TUN/TAP device driver, 1.6
tun: (C) 1999-2004 Max Krasnyansky <[email protected]>
sky2: driver version 1.30
ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
ehci-pci: EHCI PCI platform driver
ehci-platform: EHCI generic platform driver
ohci_hcd: USB 1.1 'Open' Host Controller (OHCI) Driver
ohci-pci: OHCI PCI platform driver
ohci-platform: OHCI generic platform driver
usbcore: registered new interface driver usb-storage
mousedev: PS/2 mouse device common for all mice
sdhci: Secure Digital Host Controller Interface driver
sdhci: Copyright(c) Pierre Ossman
sdhci-pltfm: SDHCI platform and OF driver helper
usbcore: registered new interface driver usbhid
usbhid: USB HID core driver
NET: Registered protocol family 17
9pnet: Installing 9P2000 support
Key type dns_resolver registered
registered taskstats version 1
hctosys: unable to open rtc device (rtc0)
fdt: not creating '/sys/firmware/fdt' 1: CRC check failed
fdt: not creating '/sys/firmware/fdt' 2: CRC check failed
Entering initrd_load
in rd_load_image
in identify_ramdisk_image
RAMDISK: gzip image found at block 0
VFS: Mounted root (ext2 filesystem) readonly on device 1:0.
devtmpfs: mounted
in free_reserved_area
Freeing unused kernel memory: 424K (ffffffc0007e9000 - ffffffc000853000)
in free_alternatives_memory arch/arm64/kernel/alternative.c
in free_reserved_area
Freeing alternatives memory: 16K (ffffffc000853000 - ffffffc000857000)
after free_initmem init/main.c
before ramdisk_execute_command
in run_init_process init/main.c init_filename /sbin/init
in run_init_process init/main.c init_filename /etc/init
in run_init_process init/main.c init_filename /bin/init
in run_init_process init/main.c init_filename /bin/sh
Kernel panic - not syncing: No working init found. Try passing init= option to kernel. See Linux Documentation/init.txt for guidance.
CPU: 0 PID: 1 Comm: swapper/0 Not tainted 4.1.8-rt8 #26
Hardware name: LS1043A IMRA DPLF Board (DT)
Call trace:
[<ffffffc0000897ec>] dump_backtrace+0x0/0x11c
[<ffffffc000089918>] show_stack+0x10/0x1c
[<ffffffc0005b4700>] dump_stack+0x7c/0x98
[<ffffffc0005b36e0>] panic+0xe0/0x220
[<ffffffc0005b1480>] kernel_init+0xbc/0x104
---[ end Kernel panic - not syncing: No working init found. Try passing init= option to kernel. See Linux Documentation/init.txt for guidance.

0 Kudos
Reply
0 Replies