LS1028a clock frequency is reduced when the temperature increases

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LS1028a clock frequency is reduced when the temperature increases

1,423 次查看
Myth
Contributor I

I am using LS1028ardb, whenever the temperature is increasing and is between alert and critical temperature, the cpu clock frequency is reducing. I read 92deg max but the clock frequency was limited to 300MHz which makes my application unable to run. what can be the solution inorder to avoid clock frequency reduction. And I want to know wether thermal monitor unit reads temperature data from SA56004 or directly from the CPU core???

0 项奖励
回复
1 回复

1,336 次查看
MarkChapman
Contributor I

Improve cooling, optimize application for lower power usage; clarify thermal sensor source for accurate readings.

Best Wishes paybyplateMA ehallpass
0 项奖励
回复