LS1021A-TWR: Flash programming with CW

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LS1021A-TWR: Flash programming with CW

2,678件の閲覧回数
z_v
Contributor I

Hello,

Upon trying to program a new u-boot with Code Warrior I got the following messages:

fl::target -lc "LC for Simple Flash"

fl::target -b 0x10000000 0x20000
fl::target -v off -l off
cmdwin::fl::device -d "JS28F00AM29EWHA" -o "64Mx16x1" -a 0x60000000 0x67ffffff
cmdwin::fl::image -f "u-boot.bin" -t "Auto Detect" -re on -r 0x60000000 0x67ffffff -oe on -o 0x60100000
cmdwin::fl::erase image
 Beginning Operation ...   
-------------------------
Auto-detection is successful.  
  File is of type Binary/Raw Format.  
 
Performing target initialization ...   
 Downloading Flash Device Driver ...  
 Reading flash ID ...
Erasing Sector 0x60100000 to 0x6011FFFF  
Erasing Sector 0x60120000 to 0x6013FFFF  
Erasing Sector 0x60140000 to 0x6015FFFF  
Erasing Sector 0x60160000 to 0x6017FFFF  
 Erasing ...
Error:  Erase failed.   Flash driver reports the following error(s):  Sector Protection Error
Error: Erase failed. Flash driver reports the following error(s):  Sector Protection Error

Can you help ?

Till now I programmed u-boot few times and it was Ok.

Thank you,

Z.V

0 件の賞賛
返信
4 返答(返信)

2,464件の閲覧回数
z_v
Contributor I

Hi Adrian,

I double checked.

SW2,3 are set to bank 0.

Thank you,

Z.V

0 件の賞賛
返信

2,464件の閲覧回数
addiyi
NXP Employee
NXP Employee

If the switches are correct, then try to unprotect before erase/program.

Adrian

0 件の賞賛
返信

2,464件の閲覧回数
z_v
Contributor I

Hi Adrian,

I recreated the CW RAM application project.

Now programming works fine.

Thank you !

Z.V

0 件の賞賛
返信

2,464件の閲覧回数
addiyi
NXP Employee
NXP Employee

From the dip-sw make sure the IFC is enabled and QSPI is disabled.

Adrian

0 件の賞賛
返信