LS1021A SEC CRCA Dynamic Custom Mode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1021A SEC CRCA Dynamic Custom Mode

1,430 Views
Xi-nanWang
Contributor II

LS1021A, I use SEC for hardware CRC calculation, I can only run the STANDARD IEEE and IETF mode correctly, when it comes to Dynamic CUSTOM mode, the hardware will generate all ZERO results. The register configuration are the same except the mode selection AAI and Key Register. Did I miss any critical register bits? Or which registers should I consider to use CRCA dynamic custom mode?

Labels (1)
0 Kudos
Reply
1 Reply

1,311 Views
bpe
NXP Employee
NXP Employee

This is a duplicate thread.

See this post for the answer.

Regards,

Platon

0 Kudos
Reply