L2switch

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

L2switch

2,946 次查看
zilu
Contributor II

Hi,i have some questions about the intergrated switch T1040rdb.

As the following chart in attached file:
we want to match the specific packets which are untagged and ethertype is ARP of port 0. 
When matched, two actions:
1.       Add double vlan tag to untagged arp packets: vlan101+40
2.       Redirect  vlan=101 packets to port8
 
My questions are:
(1)    Does IS1 can support action 1? If not, how can we do to achieve this ?




0 项奖励
回复
1 回复

2,889 次查看
bpe
NXP Employee
NXP Employee

The switch can do what you described, but there is no way to configure  for that using the CLI tool available in  QorIQ SDK. It requires advanced features/APIs  which are not in public access. Consider NXP paid Professional  Services to create a switch configuration customized for your specific task(s):

Professional Services Software Technologies (QorIQ 2017) | NXP Semiconductors 


Have a great day,
Platon

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复