Jailhouse hypervisor support for LS1043

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Jailhouse hypervisor support for LS1043

2,448 Views
tbiernat
Contributor I

Can someone speak to (or point me in the right direction) to the state of current jailhouse support for this board? I see some jailhouse config support under arm64.

 
Thanks in advance,
Tim B
0 Kudos
Reply
3 Replies

2,303 Views
Oswalag
NXP TechSupport
NXP TechSupport

Harpoon recipes reside in meta-layer "meta-nxp-harpoon"

Please take a look on the Real-time Edge Yocto Project User Guide.

It provides a latency test application running on inmate cell of Jailhouse (running on FreeRTOS or Zephyr).

0 Kudos
Reply

2,364 Views
tbiernat
Contributor I

OK, I have LS1043A booting to a Yocto image based on RT Edge 2.3.

Able to partition using jailhouse with linux inmate.

Would like to run Harpoon Zephyr RTOS latency example. I see the layer is available, but no /usr/share/harpoon in the built image. Does this board support the Harpoon examples? Anything special I need to do in Yocto build to include this in the image?

Thanks,  Tim

0 Kudos
Reply

2,397 Views
Oswalag
NXP TechSupport
NXP TechSupport

Hello,

We have currently jailhouse support under the real-time edge software that enables real-time applications for the Layerscape products and can be easily integrated with the Yocto SDKs for these products.

Real-Time Edge Software