Is T2080RDB-PC is safe from hardware attack??

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Is T2080RDB-PC is safe from hardware attack??

1,355 次查看
leelambjae
Contributor I

Hi Hi

I am using T2080RDB-PC to research.

I have a question about T2080RDB-PC's security.

Is T2080RDB-PC is safe from cold boot attack which steals data from memory while data is remain in ram?

Also, is it safe from USB Killer which discharges 200VDC over the data lines of the host device??

THANK U

0 项奖励
回复
1 回复

1,259 次查看
ufedor
NXP Employee
NXP Employee

> Is T2080RDB-PC is safe from cold boot attack which steals data from memory while data is remain in ram?

When Secure Boot is enabled the "cold boot" attack is impossible - refer to the:

https://www.nxp.com/docs/en/brochure/PWRARBYNDBITSTA.pdf 

https://elearning.nxp.com/enrol/index.php?id=254 

 

> Also, is it safe from USB Killer which discharges 200VDC over the data lines of the host device??

USB ports of the T2080RDB are equipped with VBUS054B-HSF ESD protectors.

0 项奖励
回复