Is T2080RDB-PC is safe from hardware attack??

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is T2080RDB-PC is safe from hardware attack??

1,351件の閲覧回数
leelambjae
Contributor I

Hi Hi

I am using T2080RDB-PC to research.

I have a question about T2080RDB-PC's security.

Is T2080RDB-PC is safe from cold boot attack which steals data from memory while data is remain in ram?

Also, is it safe from USB Killer which discharges 200VDC over the data lines of the host device??

THANK U

0 件の賞賛
返信
1 返信

1,255件の閲覧回数
ufedor
NXP Employee
NXP Employee

> Is T2080RDB-PC is safe from cold boot attack which steals data from memory while data is remain in ram?

When Secure Boot is enabled the "cold boot" attack is impossible - refer to the:

https://www.nxp.com/docs/en/brochure/PWRARBYNDBITSTA.pdf 

https://elearning.nxp.com/enrol/index.php?id=254 

 

> Also, is it safe from USB Killer which discharges 200VDC over the data lines of the host device??

USB ports of the T2080RDB are equipped with VBUS054B-HSF ESD protectors.

0 件の賞賛
返信