Is PPC_DISABLE_THREADS for e6500 rev2 needed? Whats this errata?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is PPC_DISABLE_THREADS for e6500 rev2 needed? Whats this errata?

2,259件の閲覧回数
kirankumara
Contributor I

We see that PPC_DISABLE_THREADS only needed for e6500 Rev1 chip; However we see that, if we dont use this even for our Rev2 processor core, then we see that CPU get stuck in high traffic condition when the traffic is stopped after few hours; When we enable this erratum, only then, the issue goes away. however only 12 cores can be used now.

I need to know, whether this change is required for Rev2?

If we do the change, are there any side effects because we, now, get only 12 cores instead of 24 cores?

Share the errata please?

0 件の賞賛
返信
4 返答(返信)

2,167件の閲覧回数
ufedor
NXP Employee
NXP Employee

The Errata document is confidential - please create a Technical Case:

How I could create a Service Request? | NXP Community 

0 件の賞賛
返信

2,167件の閲覧回数
kirankumara
Contributor I

Hello,

I  want to know if this errata fix is needed for us first up. Can you reply for that?

What more info you need for technical case than this? Hiw do we create it?

Regards,

Kiran

0 件の賞賛
返信

2,167件の閲覧回数
ufedor
NXP Employee
NXP Employee

It is not obvious which hardware erratrum (or errata) is causing the issue, so additional investigation is needed.

> What more info you need for technical case than this?

Please provide a technical explanation of the issue reproducibility.

> Hiw do we create it?

Please refer to the link in the first response.

0 件の賞賛
返信

2,167件の閲覧回数
kirankumara
Contributor I

Hello,

Ours is t4240 rev2. In that case this errata holds good? If so, what would be the fix?

I will try to create technical case today.

Regards,

Kiran

0 件の賞賛
返信