When the T2081 fetch its RCW, SerDes1 PLL 1 is not locking because we supply 100MHz on
SD1_CLK1 and SD1_CLK2. (HRST_REQn asserted after RCW read from NOR Flash)
- We need PCIe4_x4 Gen3 and PCIe3_x4 Gen2.
Do you have a workaround to operate with SD1_CLK1 and SD1_CLK2 at 100MHz ?
I can live with PCIe4_x4 Gen2 (in place of Gen3)
NOTA : In our design we are not able to supply 155MHz on SD1_CLK1
Hello,
Find attached the new RCW patched
Additional relevant info.
I read the DCFG_CCSR_PORSR1 register and I get value = 0x13ffff7f.
with XVDD_SEL = '0'. This looks to me wrong, I am expecting '1' because
T2081 pin ASLEEP has a 4K7 pull-up resistor and should configure XVDD_SEL = '1'.
The SD1_CLK1=100MHz is a valid clock for the SRDS_PR TCL_S1 =0xAA - refer to the QorIQ T2080 Reference Manual, Table 19-4. Valid SerDes Reference Clocks and RCW Encodings.
Please provide binary image of the RCW being used.
Confirm that you have checked that the RCW is correctly read from its source.
Hello,
YES, the RCW is read correctly, we have verified it at the IFC Bus level and also confirmed by UBOOT.
NOTA : To have UBOOT up and running I do not use HRST_REQn -> HRSTn to the T2081
I am using following file .rcw to generate the RCW
/*
* T2081QDS RCW for SerDes Protocol 0xAA
*
* 2G configuration -- 2 RGMII + PCIE x4 (slot1) + PCIE x4 (slot2)
*
* Frequencies:
*
* SYSCLK: 66.66 MHz (SW3[1:4] = 0000)
* DDRCLK: 133.33MHz (SW3[5:6] = 11)
* SD1_REF1 CLK: 156.25 MHz (SW4[1:2] = 10)
* SD1_REF2 CLK: 100 MHz (SW4[3:4] = 11)
* SD2_REF1 CLK: 100 MHz (SW4[5:6] = 11)
* SD2_REF2 CLK: 100 MHz (SW4[7:8] = 11)
*
* Core -- 1200 MHz (Mul 18)
* Platform -- 533 MHz (Mul 8)
* DDR -- 800 MHz (1600 MT/s) (Mul 12)
* FMAN -- 533 MHz (HWA_CGA_M1_CLK_SEL=5)
*
* RGMII1: MAC3
* RGMII2: MAC4
* XFI: NULL
*
* Slot Card
* 1 PCIe4 x4 (8/5/2.5 Gbps)
* 2 PCIe3 x4 (5/2.5 Gbps)
* 3 NULL
* 4 NULL
* 5 NULL
* 6 NULL
* 7 NULL
*
* PBI source is NOR
*/
#include <../t2080qds/t2080.rcwi>
SYS_PLL_RAT=8
MEM_PLL_RAT=12
CGA_PLL1_RAT=18
CGA_PLL2_RAT=21
HWA_CGA_M1_CLK_SEL=5
HWA_CGA_M2_CLK_SEL=4
FM_MAC_RAT=1
SRDS_PLL_PD_S1=0
SRDS_PRTCL_S1=0xaa
SRDS_PLL_REF_CLK_SEL_S1=0
SRDS_DIV_PEX_S1=0
PBI_SRC=14
BOOT_LOC=24
IFC_MODE=39
DRAM_LAT=1
UART_BASE=6
IRQ_BASE=511
Regards
Joel