How to program a NOR Flash using JTAG ins LS2085aqds board?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to program a NOR Flash using JTAG ins LS2085aqds board?

1,604件の閲覧回数
pratikbhatt
Contributor II

I have LS2085aqds reference board. From that suppose i make a my own custom board. So while booting up first time how i program the NOR flash using JTAG for NOR flash booting. Is there any DIP switch setting i have to change or I have to download a special software or something?

0 件の賞賛
返信
1 返信

1,453件の閲覧回数
r8070z
NXP Employee
NXP Employee


Have a great day,

Freescale provides CodeWarrior software tool

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=CW-LS-ARM8

and JTAG emulator (target probe) CodeWarrior TAP

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=CW_TAP

CodeWarrior includes Flash Programmer which control LS2085 based board via CodeWarrior TAP and permit program board’s flash memory.

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信