How to implement intercore communicating by use dpaa in b4860

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to implement intercore communicating by use dpaa in b4860

1,909 Views
nguyentrieulang
Contributor I

Hi,

I am using b4860. I try to modify source code of dpaa_demo for intercore communicating by replace dedicate channel by pool channel but it is not success. Anyone can help me, please !!!

0 Kudos
Reply
2 Replies

1,760 Views
lunminliang
NXP Employee
NXP Employee

Hello Nguyen Trieu Lang

Are you trying to implement intercore communication among SC3900 cores?

Can you please specify what code have you changed and what is the failure?

Regards

Lunmin

0 Kudos
Reply

1,760 Views
nguyentrieulang
Contributor I

hi Lunmin,

I modify source code of dpaa_demo project at :CW_SC_3900FP_v10.8.3\SC\StarCore_Support\SmartDSP\demos\starcore\b4860\dpaa_demo.

Now I can implement intercore communication but it is success only by using dedicate channel. For example ,  if I want to send message from core 0 to core 1. For core 0, i must set qman_fqr_params->channel =1 at function appInitQmanFqrParams.

But if i want to use pool channel , when i set qman_fqr_params->channel = (qm_fq_channel_t)(E_QM_FQ_CHANNEL_POOL1) in both core. it is n't success.

Brs,

Lang

0 Kudos
Reply