How to implement intercore communicating by use dpaa in b4860

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to implement intercore communicating by use dpaa in b4860

1,908件の閲覧回数
nguyentrieulang
Contributor I

Hi,

I am using b4860. I try to modify source code of dpaa_demo for intercore communicating by replace dedicate channel by pool channel but it is not success. Anyone can help me, please !!!

0 件の賞賛
返信
2 返答(返信)

1,759件の閲覧回数
lunminliang
NXP Employee
NXP Employee

Hello Nguyen Trieu Lang

Are you trying to implement intercore communication among SC3900 cores?

Can you please specify what code have you changed and what is the failure?

Regards

Lunmin

0 件の賞賛
返信

1,759件の閲覧回数
nguyentrieulang
Contributor I

hi Lunmin,

I modify source code of dpaa_demo project at :CW_SC_3900FP_v10.8.3\SC\StarCore_Support\SmartDSP\demos\starcore\b4860\dpaa_demo.

Now I can implement intercore communication but it is success only by using dedicate channel. For example ,  if I want to send message from core 0 to core 1. For core 0, i must set qman_fqr_params->channel =1 at function appInitQmanFqrParams.

But if i want to use pool channel , when i set qman_fqr_params->channel = (qm_fq_channel_t)(E_QM_FQ_CHANNEL_POOL1) in both core. it is n't success.

Brs,

Lang

0 件の賞賛
返信