Hi, Let us know if nxp provides the BSP for "RD_P1020WLANS: QorIQ P1020-WLAN Access Point/Router" that can supports on OpenWrt.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Hi, Let us know if nxp provides the BSP for "RD_P1020WLANS: QorIQ P1020-WLAN Access Point/Router" that can supports on OpenWrt.

790件の閲覧回数
niranjankumar
Contributor I

@niranjan.kumar@logic-fruit.com,@dhruv.saxena@logic-fruit.com,

Does NXP or any other third part provides the complete board package for the below mentioned board which will be compatible with the OpenWrt. If it is, please gives the deatils of BSP and the link from where we can get it.

Board Deatils:

RD_P1020WLANS: QorIQ P1020-WLAN Access Point/Router

Thanks,

0 件の賞賛
返信
1 返信

661件の閲覧回数
Pavel
NXP Employee
NXP Employee

NXP offers LTIB Linux BSP for this board:

http://www.nxp.com/products/microcontrollers-and-processors/power-architecture-processors/qoriq-plat...

 

Find the "P1020 WLAN Software Bundle(REV 0)" on this page.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信