GPIO sample program for QorIQ Processor

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

GPIO sample program for QorIQ Processor

1,044 Views
nareshpuli
Contributor III

GPIO  Smple program for QorIQ Processor, how  we enable & disable Pins

0 Kudos
Reply
2 Replies

845 Views
r8070z
NXP Employee
NXP Employee

Have a great day,

Please see  On P2020, GPIO[0:4] is multiplexed with IRQ[7:11]. How does software configure it usage so that it ... 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

845 Views
nareshpuli
Contributor III

thanks,

i want write a program in ubuntu, what are header files  of  QorlQ P2020 .

Regards

Naresh

0 Kudos
Reply