FloTherm model for T2080

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FloTherm model for T2080

1,515 Views
xmalbadi
Contributor I

I need the FloTherm model of the T2080. I am actually using FloTherm XT, but as far as I know the model is only available for FloTherm.

0 Kudos
Reply
1 Reply

1,406 Views
ufedor
NXP Employee
NXP Employee

The model could be provided when the following pre-requisites are fulfilled:

1) it is needed to create a Technical Case using your company's email:

How I could create a Service Request? 

2) in the Technical Case it is required to provide a confirmation that your company has active signed NDA with NXP.

The NDA can be arranged by contacting one of NXP authorized distributors and asking to have a NDA for specific product or technology.
The Distributor network can be found at:
http://www.nxp.com/support/sample-buy/distributor-network:DISTRIBUTORS

0 Kudos
Reply