File System Mount Question

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

File System Mount Question

4,126 Views
leelambjae
Contributor I

Hi 

Sorry for asking similar questions, but it still didn't work  :,(

 

We asked about root file system mount again.

 

Last question, we got the answer that bootm command contains incorrect address for root file system.

Out bootscript is as follows:

  bootscript

we refer to SDK. and normal booting works well. 

So we think that u-boot-secure-boot has problem. is this right?? answer PLZ

If u-boot-secure-boot has problem, we have to change u-boot-secure-boot. 

In this process, do we have to change secure u-boot based on sdk u-boot source code? or can secure u-boot changed based on u-boot of DENX?

When we change secure u-boot, do we have to change secure u-boot based on sdk u-boot source code? Or can secure u-boot changed based on u-boot of DENX?

=> pri
baudrate=115200
bdev=sda3
bootcmd=setenv bs_hdraddr 0xe8e00000;setenv bootargs 'root=/dev/ram rw console=ttyS0,115200 ramdisk_size=600000';esbc_validate $bs_hdraddr;source $img_addr;esbc_halt
bootdelay=0
bootfile=uImage
consoledev=ttyS0
ethact=FM1@DTSEC3
ethprime=FM1@DTSEC3
fdtaddr=1e00000
fdtfile=t2080rdb/t2080rdb.dtb
fman_ucode=eff00000
hwconfig=fsl_ddr:ctlr_intlv=cacheline,bank_intlv=auto;usb1:dr_mode=host,phy_type=utmi
initrd_high=0xffffffff
loadaddr=1000000
netdev=eth0
nfsboot=setenv bootargs root=/dev/nfs rw nfsroot=$serverip:$rootpath ip=$ipaddr:$serverip:$gatewayip:$netmask:$hostname:$netdev:off console=$consoledev,$baudrate $othbr
ramboot=setenv bootargs root=/dev/ram rw console=$consoledev,$baudrate $othbootargs;tftp $ramdiskaddr $ramdiskfile;tftp $loadaddr $bootfile;tftp $fdtaddr $fdtfile;bootr
ramdiskaddr=2000000
ramdiskfile=t2080rdb/ramdisk.uboot
rootpath=/opt/nfsroot
stderr=serial
stdin=serial
stdout=serial
tftpflash=tftpboot $loadaddr $uboot && protect off $ubootaddr +$filesize && erase $ubootaddr +$filesize && cp.b $loadaddr $ubootaddr $filesize && protect on $ubootaddre
uboot="u-boot.bin"
ubootaddr=0xeff40000

Environment size: 1360/8188 bytes
=> help
? - alias for 'help'
base - print or set address offset
bdinfo - print Board Info structure
blob - Blob encapsulation/decryption
boot - boot default, i.e., run 'bootcmd'
bootd - boot default, i.e., run 'bootcmd'
bootelf - Boot from an ELF image in memory
bootm - boot application image from memory
bootp - boot image via network using BOOTP/TFTP protocol
bootvx - Boot vxWorks from an ELF image
chpart - change active partition
cmp - memory compare
coninfo - print console devices and information
cp - memory copy
cpld - Reset the board or alternate bank
cpu - Multiprocessor CPU boot manipulation and release
crc32 - checksum calculation
dhcp - boot image via network using DHCP/TFTP protocol
dm - Driver model low level access
echo - echo args to console
editenv - edit environment variable
env - environment handling commands
erase - erase FLASH memory
errata - Report errata workarounds
esbc_halt- Put the core in spin loop (Secure Boot Only)
esbc_validate- Validates signature on a given image using RSA verification
exit - exit script
ext2load- load binary file from a Ext2 filesystem
ext2ls - list files in a directory (default /)
false - do nothing, unsuccessfully
fatinfo - print information about filesystem
fatload - load binary file from a dos filesystem
fatls - list files in a directory (default /)
fatsize - determine a file's size
fdt - flattened device tree utility commands
flinfo - print FLASH memory information
go - start application at address 'addr'
hash - compute hash message digest
help - print command description/usage
i2c - I2C sub-system
iminfo - print header information for application image
imls - list all images found in flash
imxtract- extract a part of a multi-image
itest - return true/false on integer compare
loadb - load binary file over serial line (kermit mode)
loads - load S-Record file over serial line
loadx - load binary file over serial line (xmodem mode)
loady - load binary file over serial line (ymodem mode)
loop - infinite loop on address range
mac - display and program the system ID and MAC addresses in EEPROM
md - memory display
mdio - MDIO utility commands
mii - MII utility commands
mm - memory modify (auto-incrementing address)
mmc - MMC sub system
mmcinfo - display MMC info
mtdparts- define flash/nand partitions
mtest - simple RAM read/write test
mw - memory write (fill)
nand - NAND sub-system
nboot - boot from NAND device
nfs - boot image via network using NFS protocol
nm - memory modify (constant address)
pci - list and access PCI Configuration Space
ping - send ICMP ECHO_REQUEST to network host
printenv- print environment variables
protect - enable or disable FLASH write protection
reginfo - print register information
reset - Perform RESET of the CPU
run - run commands in an environment variable
sata - SATA sub system
setenv - set environment variables
setexpr - set environment variable as the result of eval expression
sf - SPI flash sub-system
showvar - print local hushshell variables
sleep - delay execution for some time
source - run script from memory
test - minimal test like /bin/sh
tftpboot- boot image via network using TFTP protocol
true - do nothing, successfully
usb - USB sub-system
usbboot - boot from USB device
vdd_override- override VDD
vdd_read- read VDD
version - print monitor, compiler and linker version

This is u-boot.env

U-Boot 2016.092.0+ga06b209 (Jul 13 2018 - 03:47:47 -0700)

CPU0: T2080E, Version: 1.1, (0x85380011)
Core: e6500, Version: 2.0, (0x80400120)
Clock Configuration:
CPU0:1799.820 MHz, CPU1:1799.820 MHz, CPU2:1799.820 MHz, CPU3:1799.820 MHz,
CCB:599.940 MHz,
DDR:933.310 MHz (1866.620 MT/s data rate) (Asynchronous), IFC:599.940 MHz
FMAN1: 699.930 MHz
QMAN: 299.970 MHz
PME: 599.940 MHz
L1: D-cache 32 KiB enabled
I-cache 32 KiB enabled
Reset Configuration Word (RCW):
00000000: 1207001b 15000000 00000000 00000000
00000010: 66150002 00000000 ec627000 c1000000
00000020: 00800000 00000000 00000000 000307fc
00000030: 00000000 00000000 00000000 00000004
Board: T2080RDB, Board rev: 0x01 CPLD ver: 0x06, boot from NOR vBank4
SERDES Reference Clocks:
SD1_CLK1=156.25MHZ, SD1_CLK2=100.00MHZ
SD2_CLK1=100.00MHZ, SD2_CLK2=100.00MHZ
I2C: ready
SPI: ready
DRAM: Initializing....using SPD
Detected UDIMM D3XP56082XL10AA
2 GiB left unmapped
4 GiB (DDR3, 64-bit, CL=13, ECC on)
DDR Chip-Select Interleaving Mode: CS0+CS1
VID: Core voltage after adjustment is at 1023 mV
Flash: 128 MiB
L2: 2 MiB enabled
Corenet Platform Cache: 512 KiB enabled
Using SERDES1 Protocol: 102 (0x66)
Using SERDES2 Protocol: 21 (0x15)
SEC0: RNG instantiated
NAND: 512 MiB
MMC: FSL_SDHC: 0
Using default environment

EEPROM: Invalid ID (ff ff ff ff)
PCIe1: Endpoint, undetermined, regs @ 0xfe240000
PCIe1: Bus 00 - 00
PCIe2: Root Complex, x1 gen1, regs @ 0xfe250000
PCIe2: Bus 01 - 02
PCIe3: disabled
PCIe4: Root Complex, no link, regs @ 0xfe270000
PCIe4: Bus 03 - 03
In: serial
Out: serial
Err: serial
Net: Fman1: Uploading microcode version 106.4.18
Could not get PHY for FM_TGEC_MDIO: addr 12
Failed to connect
Could not get PHY for FM_TGEC_MDIO: addr 13
Failed to connect
FM1@DTSEC3 [PRIME]
Error: FM1@DTSEC3 address not set.
, FM1@DTSEC4
Error: FM1@DTSEC4 address not set.
, FM1@TGEC1
Error: FM1@TGEC1 address not set.
, FM1@TGEC2
Error: FM1@TGEC2 address not set.
, FM1@TGEC3
Error: FM1@TGEC3 address not set.
, FM1@TGEC4
Error: FM1@TGEC4 address not set.

Hit any key to stop autoboot: 0
esbc_validate command successful
## Executing script at e8a00000
uImage validate start
esbc_validate command successful
uImage validate end
dtb validate start
esbc_validate command successful
dtb validate end
rootfs validate start
esbc_validate command successful
rootfs validate end
WARNING: adjusting available memory to 30000000
## Booting kernel from Legacy Image at e8020000 ...
Image Name: Linux-4.1.35-rt41
Image Type: PowerPC Linux Kernel Image (gzip compressed)
Data Size: 5106036 Bytes = 4.9 MiB
Load Address: 00000000
Entry Point: 00000000
Verifying Checksum ... OK
## Loading init Ramdisk from Legacy Image at e9300000 ...
Image Name: fsl-image-core-t2080rdb-20180820
Image Type: PowerPC Linux RAMDisk Image (gzip compressed)
Data Size: 33049619 Bytes = 31.5 MiB
Load Address: 00000000
Entry Point: 00000000
Verifying Checksum ... OK
## Flattened Device Tree blob at e8800000
Booting using the fdt blob at 0xe8800000
Uncompressing Kernel Image ... OK
Loading Device Tree to 03fe3000, end 03fff2c0 ... OK
Reserved memory: initialized node bman-fbpr, compatible id fsl,bman-fbpr
Reserved memory: initialized node qman-fqd, compatible id fsl,qman-fqd
Reserved memory: initialized node qman-pfdr, compatible id fsl,qman-pfdr
Reserved memory: initialized node pme-pdsr, compatible id fsl,pme-pdsr
Reserved memory: initialized node pme-sre, compatible id fsl,pme-sre
Using CoreNet Generic machine description
MMU: Supported page sizes
4 KB as direct
2048 KB as direct & indirect
4096 KB as direct
16384 KB as direct
65536 KB as direct
262144 KB as direct
1048576 KB as direct
MMU: Book3E HW tablewalk enabled
Found initrd at 0xc0000000e9300040:0xc0000000eb284c53
bootconsole [udbg0] enabled
CPU maps initialized for 2 threads per core
Starting Linux PPC64 #1 SMP Mon Aug 20 02:48:23 PDT 2018
-----------------------------------------------------
ppc64_pft_size = 0x0
phys_mem_size = 0x100000000
dcache_line_size = 0x40
icache_line_size = 0x40
cpu_features = 0x00180480581802c8
possible = 0x00180480581802c8
always = 0x00180400581802c0
cpu_user_features = 0xdc008000 0x08000000
mmu_features = 0x000a0010
firmware_features = 0x0000000000000000
-----------------------------------------------------
<- setup_system()
Linux version 4.1.35-rt41 (add@ubuntu) (gcc version 4.9.2 (GCC) ) #1 SMP Mon Aug 20 02:48:23 PDT 2018
CoreNet Generic board
Zone ranges:
DMA [mem 0x0000000000000000-0x000000007fffffff]
DMA32 empty
Normal [mem 0x0000000080000000-0x00000000ffffffff]
Movable zone start for each node
Early memory node ranges
node 0: [mem 0x0000000000000000-0x00000000ffffffff]
Initmem setup node 0 [mem 0x0000000000000000-0x00000000ffffffff]
MMU: Allocated 2112 bytes of context maps for 255 contexts
PERCPU: Embedded 17 pages/cpu @c0000000ffe00000 s28760 r0 d40872 u131072
Built 1 zonelists in Zone order, mobility grouping on. Total pages: 1034240
Kernel command line: root=/dev/ram rw console=ttyS0,115200 ramdisk_size=600000
log_buf_len individual max cpu contribution: 4096 bytes
log_buf_len total cpu_extra contributions: 28672 bytes
log_buf_len min size: 16384 bytes
log_buf_len: 65536 bytes
early log buf free: 12032(73%)
PID hash table entries: 4096 (order: 3, 32768 bytes)
Dentry cache hash table entries: 524288 (order: 10, 4194304 bytes)
Inode-cache hash table entries: 262144 (order: 9, 2097152 bytes)
Sorting __ex_table...
Memory: 3933580K/4194304K available (7872K kernel code, 1140K rwdata, 3004K rodata, 360K init, 764K bss, 260724K reserved, 0K cma-reserved)
Hierarchical RCU implementation.
RCU debugfs-based tracing is enabled.
CONFIG_RCU_FANOUT set to non-default value of 32
Additional per-CPU info printed with stalls.
RCU restricting CPUs from NR_CPUS=24 to nr_cpu_ids=8.
RCU: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=8
NR_IRQS:512 nr_irqs:512 16
mpic: Setting up MPIC " OpenPIC " version 1.2 at ffe040000, max 8 CPUs
mpic: ISU size: 512, shift: 9, mask: 1ff
mpic: Initializing for 512 sources
clocksource timebase: mask: 0xffffffffffffffff max_cycles: 0x8a5d528ca, max_idle_ns: 440795203517 ns
clocksource: timebase mult[1aab5972] shift[24] registered
Console: colour dummy device 80x25
pid_max: default: 32768 minimum: 301
Mount-cache hash table entries: 8192 (order: 4, 65536 bytes)
Mountpoint-cache hash table entries: 8192 (order: 4, 65536 bytes)
e6500 family performance monitor hardware support registered
Brought up 8 CPUs
devtmpfs: initialized
clocksource jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns
xor: measuring software checksum speed
8regs : 3567.000 MB/sec
8regs_prefetch: 3156.000 MB/sec
32regs : 3005.000 MB/sec
32regs_prefetch: 2657.000 MB/sec
altivec : 5652.000 MB/sec
xor: using function: altivec (5652.000 MB/sec)
NET: Registered protocol family 16
Bman ver:0a02,02,01
qman-fqd addr 0x00000000ff000000 size 0x800000
qman-pfdr addr 0x00000000fc000000 size 0x2000000
Qman ver:0a01,03,01,02
Machine: fsl,T2080RDB
SoC family: QorIQ T2080
SoC ID: svr:0x85380011, Revision: 1.1
Can't find hose for PCI bus 0!
EDAC PCI0: Giving out device to module MPC85xx_edac controller mpc85xx_pci_err: DEV ffe240000.pcie (INTERRUPT)
MPC85xx_edac acquired irq 20 for PCI Err
MPC85xx_edac PCI err registered
platform ffe240000.pcie:pcie@0: Invalid size 0xfffff9 for dma-range
Found FSL PCI host bridge at 0x0000000ffe250000. Firmware bus number: 0->1
PCI host bridge /pcie@ffe250000 ranges:
MEM 0x0000000c20000000..0x0000000c2fffffff -> 0x00000000e0000000
IO 0x0000000ff8010000..0x0000000ff801ffff -> 0x0000000000000000
/pcie@ffe250000: PCICSRBAR @ 0xff000007
setup_pci_atmu: end of DRAM 100000000
/pcie@ffe250000: Setup 64-bit PCI DMA window
/pcie@ffe250000: WARNING: Outbound window cfg leaves gaps in memory map. Adjusting the memory map could reduce unnecessary bounce buffering.
/pcie@ffe250000: DMA window size is 0xe0000000
EDAC PCI1: Giving out device to module MPC85xx_edac controller mpc85xx_pci_err: DEV ffe250000.pcie (INTERRUPT)
MPC85xx_edac acquired irq 21 for PCI Err
MPC85xx_edac PCI err registered
platform ffe250000.pcie:pcie@0: Invalid size 0xfffff9 for dma-range
Found FSL PCI host bridge at 0x0000000ffe270000. Firmware bus number: 0->0
PCI host bridge /pcie@ffe270000 ranges:
MEM 0x0000000c40000000..0x0000000c4fffffff -> 0x00000000e0000000
IO 0x0000000ff8030000..0x0000000ff803ffff -> 0x0000000000000000
/pcie@ffe270000: PCICSRBAR @ 0xff000007
setup_pci_atmu: end of DRAM 100000000
/pcie@ffe270000: Setup 64-bit PCI DMA window
/pcie@ffe270000: WARNING: Outbound window cfg leaves gaps in memory map. Adjusting the memory map could reduce unnecessary bounce buffering.
/pcie@ffe270000: DMA window size is 0xe0000000
EDAC PCI2: Giving out device to module MPC85xx_edac controller mpc85xx_pci_err: DEV ffe270000.pcie (INTERRUPT)
MPC85xx_edac acquired irq 23 for PCI Err
MPC85xx_edac PCI err registered
platform ffe270000.pcie:pcie@0: Invalid size 0xfffff9 for dma-range
software IO TLB [mem 0xf2e00000-0xf6e00000] (64MB) mapped at [c0000000f2e00000-c0000000f6dfffff]
PCI: Probing PCI hardware
fsl-pci ffe250000.pcie: PCI host bridge to bus 0001:00
pci_bus 0001:00: root bus resource [io 0x10000-0x1ffff] (bus address [0x0000-0xffff])
pci_bus 0001:00: root bus resource [mem 0xc20000000-0xc2fffffff] (bus address [0xe0000000-0xefffffff])
pci_bus 0001:00: root bus resource [bus 00-01]
pci 0001:00:00.0: [Firmware Bug]: reg 0x10: invalid BAR (can't size)
pci 0001:00:00.0: PCI bridge to [bus 01-ff]
fsl-pci ffe270000.pcie: PCI host bridge to bus 0002:00
pci_bus 0002:00: root bus resource [io 0x21000-0x30fff] (bus address [0x0000-0xffff])
pci_bus 0002:00: root bus resource [mem 0xc40000000-0xc4fffffff] (bus address [0xe0000000-0xefffffff])
pci_bus 0002:00: root bus resource [bus 00]
pci 0002:00:00.0: [Firmware Bug]: reg 0x10: invalid BAR (can't size)
pci 0002:00:00.0: bridge configuration invalid ([bus 00-00]), reconfiguring
pci 0002:00:00.0: PCI bridge to [bus 01-ff]
PCI: Cannot allocate resource region 6 of device 0001:00:00.0, will remap
pci 0001:00:00.0: BAR 6: no space for [mem size 0x01000000 pref]
pci 0001:00:00.0: BAR 6: failed to assign [mem size 0x01000000 pref]
pci 0001:00:00.0: PCI bridge to [bus 01]
pci 0001:00:00.0: bridge window [io 0x10000-0x1ffff]
pci 0001:00:00.0: bridge window [mem 0xc20000000-0xc2fffffff]
pci 0002:00:00.0: BAR 6: no space for [mem size 0x01000000 pref]
pci 0002:00:00.0: BAR 6: failed to assign [mem size 0x01000000 pref]
pci 0002:00:00.0: PCI bridge to [bus 01]
pci 0002:00:00.0: bridge window [io 0x21000-0x30fff]
pci 0002:00:00.0: bridge window [mem 0xc40000000-0xc4fffffff]
raid6: altivecx1 gen() 1105 MB/s
raid6: altivecx2 gen() 1849 MB/s
raid6: altivecx4 gen() 3051 MB/s
raid6: altivecx8 gen() 2967 MB/s
raid6: int64x1 gen() 518 MB/s
raid6: int64x1 xor() 766 MB/s
raid6: int64x2 gen() 872 MB/s
raid6: int64x2 xor() 906 MB/s
raid6: int64x4 gen() 1321 MB/s
raid6: int64x4 xor() 1018 MB/s
raid6: int64x8 gen() 1159 MB/s
raid6: int64x8 xor() 826 MB/s
raid6: using algorithm altivecx4 gen() 3051 MB/s
raid6: using intx1 recovery algorithm
vgaarb: loaded
SCSI subsystem initialized
usbcore: registered new interface driver usbfs
usbcore: registered new interface driver hub
usbcore: registered new device driver usb
pps_core: LinuxPPS API ver. 1 registered
pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <[email protected]>
PTP clock support registered
EDAC MC: Ver: 3.0.0
bman-fbpr addr 0x00000000fe000000 size 0x1000000
Bman err interrupt handler present
Bman portal initialised, cpu 0
Bman portal initialised, cpu 1
Bman portal initialised, cpu 2
Bman portal initialised, cpu 3
Bman portal initialised, cpu 4
Bman portal initialised, cpu 5
Bman portal initialised, cpu 6
Bman portal initialised, cpu 7
Bman portals initialised
Qman err interrupt handler present
QMan: Allocated lookup table at 8000000000002000, entry count 131073
Qman portal initialised, cpu 0
Qman portal initialised, cpu 1
Qman portal initialised, cpu 2
Qman portal initialised, cpu 3
Qman portal initialised, cpu 4
Qman portal initialised, cpu 5
Qman portal initialised, cpu 6
Qman portal initialised, cpu 7
Qman portals initialised
Bman: BPID allocator includes range 32:32
Qman: FQID allocator includes range 256:512
Qman: FQID allocator includes range 32768:32768
Qman: CGRID allocator includes range 0:256
Qman: pool channel allocator includes range 1025:15
No USDPAA memory, no 'fsl,usdpaa-mem' in device-tree
fsl-ifc ffe124000.localbus: Freescale Integrated Flash Controller
fsl-ifc ffe124000.localbus: IFC version 1.3, 8 banks
Switched to clocksource timebase
NET: Registered protocol family 2
TCP established hash table entries: 32768 (order: 6, 262144 bytes)
TCP bind hash table entries: 32768 (order: 7, 524288 bytes)
TCP: Hash tables configured (established 32768 bind 32768)
UDP hash table entries: 2048 (order: 4, 65536 bytes)
UDP-Lite hash table entries: 2048 (order: 4, 65536 bytes)
NET: Registered protocol family 1
RPC: Registered named UNIX socket transport module.
RPC: Registered udp transport module.
RPC: Registered tcp transport module.
RPC: Registered tcp NFSv4.1 backchannel transport module.
Trying to unpack rootfs image as initramfs...
rootfs image is not initramfs (junk in compressed archive); looks like an initrd
Freeing initrd memory: 32268K (c0000000e9301000 - c0000000eb284000)
futex hash table entries: 2048 (order: 5, 131072 bytes)
audit: initializing netlink subsys (disabled)
audit: type=2000 audit(1.800:1): initialized
HugeTLB registered 4 MB page size, pre-allocated 0 pages
HugeTLB registered 16 MB page size, pre-allocated 0 pages
HugeTLB registered 64 MB page size, pre-allocated 0 pages
HugeTLB registered 256 MB page size, pre-allocated 0 pages
HugeTLB registered 1 GB page size, pre-allocated 0 pages
NFS: Registering the id_resolver key type
Key type id_resolver registered
Key type id_legacy registered
ntfs: driver 2.1.32 [Flags: R/O].
jffs2: version 2.2. (NAND) �© 2001-2006 Red Hat, Inc.
async_tx: api initialized (async)
io scheduler noop registered
io scheduler deadline registered
io scheduler cfq registered (default)
Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled
console [ttyS0] disabled
serial8250.0: ttyS0 at MMIO 0xffe11c500 (irq = 36, base_baud = 18748125) is a 16550A
console [ttyS0] enabled
console [ttyS0] enabled
bootconsole [udbg0] disabled
bootconsole [udbg0] disabled
serial8250.0: ttyS1 at MMIO 0xffe11c600 (irq = 36, base_baud = 18748125) is a 16550A
serial8250.0: ttyS2 at MMIO 0xffe11d500 (irq = 37, base_baud = 18748125) is a 16550A
serial8250.0: ttyS3 at MMIO 0xffe11d600 (irq = 37, base_baud = 18748125) is a 16550A
ePAPR hypervisor byte channel driver
brd: module loaded
loop: module loaded
st: Version 20101219, fixed bufsize 32768, s/g segs 256
fsl-sata ffe220000.sata: Sata FSL Platform/CSB Driver init
scsi host0: sata_fsl
ata1: SATA max UDMA/133 irq 68
fsl-sata ffe221000.sata: Sata FSL Platform/CSB Driver init
scsi host1: sata_fsl
ata2: SATA max UDMA/133 irq 69
fe8000000.nor: Found 1 x16 devices at 0x0 in 16-bit bank. Manufacturer ID 0x000089 Chip ID 0x00227e
Amd/Fujitsu Extended Query Table at 0x0040
Amd/Fujitsu Extended Query version 1.3.
number of CFI chips: 1
nand: device found, Manufacturer ID: 0x2c, Chip ID: 0xac
nand: Micron MT29F4G08ABBDAH4
nand: 512 MiB, SLC, erase size: 128 KiB, page size: 2048, OOB size: 64
Bad block table found at page 262080, version 0x01
Bad block table found at page 262016, version 0x01
fsl,ifc-nand fff800000.nand: IFC NAND device at 0xfff800000, bank 1
fsl_espi ffe110000.spi: cs=0, init_csmode=0x100008
m25p80 spi32766.0: found n25q512ax3, expected n25q512a
m25p80 spi32766.0: n25q512ax3 (65536 Kbytes)
fsl_espi ffe110000.spi: at 0x80000800809ae000 (irq = 53)
libphy: Fixed MDIO Bus: probed
libphy: Freescale XGMAC MDIO Bus: probed
libphy: Freescale XGMAC MDIO Bus: probed
libphy: Freescale XGMAC MDIO Bus: probed
libphy: Freescale XGMAC MDIO Bus: probed
libphy: Freescale XGMAC MDIO Bus: probed
libphy: Freescale XGMAC MDIO Bus: probed
libphy: Freescale XGMAC MDIO Bus: probed
libphy: Freescale XGMAC MDIO Bus: probed
libphy: Freescale XGMAC MDIO Bus: probed
libphy: Freescale XGMAC MDIO Bus: probed
Freescale FM module, FMD API version 21.1.0
Freescale FM Ports module
fsl_mac: fsl_mac: FSL FMan MAC API based driver
fsl_mac ffe4e0000.ethernet: of_get_mac_address(/soc@ffe000000/fman@400000/ethernet@e0000) failed
fsl_mac: probe of ffe4e0000.ethernet failed with error -22
fsl_mac ffe4e2000.ethernet: of_get_mac_address(/soc@ffe000000/fman@400000/ethernet@e2000) failed
fsl_mac: probe of ffe4e2000.ethernet failed with error -22
fsl_mac ffe4e4000.ethernet: of_get_mac_address(/soc@ffe000000/fman@400000/ethernet@e4000) failed
fsl_mac: probe of ffe4e4000.ethernet failed with error -22
fsl_mac ffe4e6000.ethernet: of_get_mac_address(/soc@ffe000000/fman@400000/ethernet@e6000) failed
fsl_mac: probe of ffe4e6000.ethernet failed with error -22
fsl_mac ffe4f0000.ethernet: of_get_mac_address(/soc@ffe000000/fman@400000/ethernet@f0000) failed
fsl_mac: probe of ffe4f0000.ethernet failed with error -22
fsl_mac ffe4f2000.ethernet: of_get_mac_address(/soc@ffe000000/fman@400000/ethernet@f2000) failed
fsl_mac: probe of ffe4f2000.ethernet failed with error -22
fsl_dpa: FSL DPAA Ethernet driver
fsl_dpa fsl,dpaa:ethernet@0: dev_get_drvdata(ffe4e0000.ethernet) failed
fsl_dpa: probe of fsl,dpaa:ethernet@0 failed with error -22
fsl_dpa fsl,dpaa:ethernet@1: dev_get_drvdata(ffe4e2000.ethernet) failed
fsl_dpa: probe of fsl,dpaa:ethernet@1 failed with error -22
fsl_dpa fsl,dpaa:ethernet@2: dev_get_drvdata(ffe4e4000.ethernet) failed
fsl_dpa: probe of fsl,dpaa:ethernet@2 failed with error -22
fsl_dpa fsl,dpaa:ethernet@3: dev_get_drvdata(ffe4e6000.ethernet) failed
fsl_dpa: probe of fsl,dpaa:ethernet@3 failed with error -22
fsl_dpa fsl,dpaa:ethernet@8: dev_get_drvdata(ffe4f0000.ethernet) failed
fsl_dpa: probe of fsl,dpaa:ethernet@8 failed with error -22
fsl_dpa fsl,dpaa:ethernet@9: dev_get_drvdata(ffe4f2000.ethernet) failed
fsl_dpa: probe of fsl,dpaa:ethernet@9 failed with error -22
fsl_advanced: FSL DPAA Advanced drivers:
fsl_proxy: FSL DPAA Proxy initialization driver
fsl_dpa_shared: FSL DPAA Shared Ethernet driver
fsl_dpa_macless: FSL DPAA MACless Ethernet driver
fsl_oh: FSL FMan Offline Parsing port driver
e1000e: Intel(R) PRO/1000 Network Driver - 2.3.2-k
e1000e: Copyright(c) 1999 - 2014 Intel Corporation.
fsl-of-dma ffe100300.dma: dma channel dma-uio0-0 initialized
fsl-of-dma ffe100300.dma: dma channel dma-uio0-1 initialized
fsl-of-dma ffe100300.dma: dma channel dma-uio0-2 initialized
fsl-of-dma ffe100300.dma: dma channel dma-uio0-3 initialized
fsl-of-dma ffe100300.dma: dma channel dma-uio0-4 initialized
fsl-of-dma ffe100300.dma: dma channel dma-uio0-5 initialized
fsl-of-dma ffe100300.dma: dma channel dma-uio0-6 initialized
fsl-of-dma ffe100300.dma: dma channel dma-uio0-7 initialized
fsl-of-dma ffe101300.dma: dma channel dma-uio1-0 initialized
fsl-of-dma ffe101300.dma: dma channel dma-uio1-1 initialized
fsl-of-dma ffe101300.dma: dma channel dma-uio1-2 initialized
fsl-of-dma ffe101300.dma: dma channel dma-uio1-3 initialized
fsl-of-dma ffe101300.dma: dma channel dma-uio1-4 initialized
fsl-of-dma ffe101300.dma: dma channel dma-uio1-5 initialized
fsl-of-dma ffe101300.dma: dma channel dma-uio1-6 initialized
fsl-of-dma ffe101300.dma: dma channel dma-uio1-7 initialized
fsl-of-dma ffe102300.dma: dma channel dma-uio2-0 initialized
fsl-of-dma ffe102300.dma: dma channel dma-uio2-1 initialized
fsl-of-dma ffe102300.dma: dma channel dma-uio2-2 initialized
fsl-of-dma ffe102300.dma: dma channel dma-uio2-3 initialized
fsl-of-dma ffe102300.dma: dma channel dma-uio2-4 initialized
fsl-of-dma ffe102300.dma: dma channel dma-uio2-5 initialized
fsl-of-dma ffe102300.dma: dma channel dma-uio2-6 initialized
fsl-of-dma ffe102300.dma: dma channel dma-uio2-7 initialized
ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
ehci-pci: EHCI PCI platform driver
fsl-ehci fsl-ehci.0: Freescale On-Chip EHCI Host Controller
fsl-ehci fsl-ehci.0: new USB bus registered, assigned bus number 1
fsl-ehci fsl-ehci.0: irq 44, io mem 0xffe210000
ata1: No Device OR PHYRDY change,Hstatus = 0xa0000000
ata1: SATA link down (SStatus 10 SControl 300)
fsl-ehci fsl-ehci.0: USB 2.0 started, EHCI 1.00
hub 1-0:1.0: USB hub found
hub 1-0:1.0: 1 port detected
fsl-ehci fsl-ehci.1: Freescale On-Chip EHCI Host Controller
fsl-ehci fsl-ehci.1: new USB bus registered, assigned bus number 2
fsl-ehci fsl-ehci.1: irq 45, io mem 0xffe211000
ata2: No Device OR PHYRDY change,Hstatus = 0xa0000000
ata2: SATA link down (SStatus 10 SControl 300)
fsl-ehci fsl-ehci.1: USB 2.0 started, EHCI 1.00
hub 2-0:1.0: USB hub found
hub 2-0:1.0: 1 port detected
usbcore: registered new interface driver usb-storage
i2c /dev entries driver
mpc-i2c ffe118000.i2c: timeout 1000000 us
rtc-ds1307 0-0068: SET TIME!
rtc-ds1307 0-0068: rtc core: registered ds1339 as rtc0
mpc-i2c ffe118100.i2c: timeout 1000000 us
mpc-i2c ffe119000.i2c: timeout 1000000 us
mpc-i2c ffe119100.i2c: timeout 1000000 us
i2c i2c-1: Added multiplexed i2c bus 4
i2c i2c-1: Added multiplexed i2c bus 5
i2c i2c-1: Added multiplexed i2c bus 6
i2c i2c-1: Added multiplexed i2c bus 7
pca954x 1-0077: registered 4 multiplexed busses for I2C switch pca9546
md: raid6 personality registered for level 6
md: raid5 personality registered for level 5
md: raid4 personality registered for level 4
Freescale(R) MPC85xx EDAC driver, (C) 2006 Montavista Software
EDAC MC0: Giving out device to module MPC85xx_edac controller mpc85xx_mc_err: DEV mpc85xx_mc_err (INTERRUPT)
MPC85xx_edac acquired irq 490 for MC
MPC85xx_edac MC err registered
sdhci: Secure Digital Host Controller Interface driver
sdhci: Copyright(c) Pierre Ossman
sdhci-pltfm: SDHCI platform and OF driver helper
sdhci-esdhc ffe114000.sdhc: No vmmc regulator found
sdhci-esdhc ffe114000.sdhc: No vqmmc regulator found
mmc0: SDHCI controller on ffe114000.sdhc [ffe114000.sdhc] using ADMA 64-bit
platform caam_qi: Linux CAAM Queue I/F driver initialised
caam ffe300000.crypto: Instantiated RNG4 SH1
caam ffe300000.crypto: device ID = 0x0a13020000000000 (Era 6)
caam ffe300000.crypto: job rings = 4, qi = 1
caam algorithms registered in /proc/crypto
platform caam_qi: algorithms registered in /proc/crypto
caam_jr ffe301000.jr: registering rng-caam
caam ffe300000.crypto: fsl,sec-v5.2 algorithms registered in /proc/crypto
usbcore: registered new interface driver usbhid
usbhid: USB HID core driver
Freescale USDPAA process driver
fsl-usdpaa: no region found
Freescale USDPAA process IRQ driver
dce_sys_init done!
fsl-dce ffe312000.dce: Device /soc@ffe000000/dce@312000 initialized ver: 0x0af00101

fsl-pme ffe316000.pme: ver: 0x00100201
Freescale pme2 db driver
Freescale pme2 scan driver
fsl-pme2-scan: device pme_scan registered
Freescale hypervisor management driver
fsl-hv: no hypervisor found
ipip: IPv4 over IPv4 tunneling driver
Initializing XFRM netlink socket
NET: Registered protocol family 10
sit: IPv6 over IPv4 tunneling driver
NET: Registered protocol family 17
NET: Registered protocol family 15
8021q: 802.1Q VLAN Support v1.8
Key type dns_resolver registered
fsl_generic: FSL DPAA Generic Ethernet driver
rtc-ds1307 0-0068: setting system clock to 2000-01-01 00:00:48 UTC (946684848)
md: Skipping autodetection of RAID arrays. (raid=autodetect will force)
RAMDISK: Couldn't find valid RAM disk image starting at 0.
List of all partitions:
0100 600000 ram0 (driver?)
0101 600000 ram1 (driver?)
0102 600000 ram2 (driver?)
0103 600000 ram3 (driver?)
0104 600000 ram4 (driver?)
0105 600000 ram5 (driver?)
0106 600000 ram6 (driver?)
0107 600000 ram7 (driver?)
0108 600000 ram8 (driver?)
0109 600000 ram9 (driver?)
010a 600000 ram10 (driver?)
010b 600000 ram11 (driver?)
010c 600000 ram12 (driver?)
010d 600000 ram13 (driver?)
010e 600000 ram14 (driver?)
010f 600000 ram15 (driver?)
1f00 131072 mtdblock0 (driver?)
1f01 524288 mtdblock1 (driver?)
1f02 65536 mtdblock2 (driver?)
No filesystem could mount root, tried: ext3 ext2 cramfs vfat ntfs
Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(1,0)
CPU: 4 PID: 1 Comm: swapper/0 Not tainted 4.1.35-rt41 #1
Call Trace:
[c0000000f10839a0] [c0000000007a7a70] .dump_stack+0xac/0xec (unreliable)
[c0000000f1083a30] [c0000000007a536c] .panic+0xf0/0x280
[c0000000f1083ad0] [c000000000aa7400] .mount_block_root+0x2fc/0x340
[c0000000f1083bb0] [c000000000aa76f8] .mount_root+0x154/0x17c
[c0000000f1083c60] [c000000000aa78f4] .prepare_namespace+0x1d4/0x234
[c0000000f1083cf0] [c000000000aa6ec4] .kernel_init_freeable+0x22c/0x26c
[c0000000f1083db0] [c0000000000021ec] .kernel_init+0x1c/0xe30
[c0000000f1083e30] [c000000000000998] .ret_from_kernel_thread+0x58/0xc0
Rebooting in 180 seconds..

This is our secure-boot log. 

0 Kudos
Reply
3 Replies

3,530 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello yangjae lee,

Please use the pre_built images provided in QorIQ-SDK-V2.0-PPCE6500-IMAGE-20160527-yocto.iso which could be downloaded from NXP public Website.

Please refer to the following procedure to sign images and create the boot script.

pastedImage_3.png

Please refer to the following NOR flash memory map for T2080RDB.

pastedImage_2.png


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

3,530 Views
leelambjae
Contributor I

Hi 

Yiping Wang.

We use 201601(64bit) ver in QorIQ-SDK-V2.0-PPCE6500-IMAGE-20160527-yocto.iso.

Now but, booting is not work at all.

Can you help us?

0 Kudos
Reply

3,530 Views
leelambjae
Contributor I

Hi 

Yiping Wang. 

Thank you for your answer.

We used pre-built image in QorIQ-SDK-V2.0-PPCE6500-IMAGE-20160527-yocto.iso. 

 

Normal booting was work well, but secure boot didn't work yet. (in 64 bits environment)

 

pastedImage_1.png

In this picture, we got the message that "rootfs image is not initramfs (junk in compressed archieved)"

Could you tell us more specifically?

THANK YOU!

HAVE A GOOD DAY!!

 

0 Kudos
Reply