ETHERNET fm1-mac3 is not visible

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ETHERNET fm1-mac3 is not visible

2,086件の閲覧回数
anshulkhare
Contributor III

Hello All,

i have T2080RDB board when i am loading kernel image .dtb and root file system i am not able to see

fm1-mac3 in logs.

i am able to see only fm1-mac9 and lo.

i am generating binary using fsl image core.

how to solve this.

Regards

Anshul

0 件の賞賛
返信
2 返答(返信)

1,943件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Hello Anshul khare,

Probably you use shared-mac dtb file, all Ethernet interfaces are assigned to USDPAA and fm1-mac9 is defined as shared-mac interface, so you only can see it in Linux.

Please use normal dtb file naming without usdpaa.


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,943件の閲覧回数
anshulkhare
Contributor III

Hello yipingwang‌

Thank you for support !!

problem is solved, i was using wrong dtb File.

Regards,

Anshul

0 件の賞賛
返信