ECCN Code

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ECCN Code

8,823件の閲覧回数
robert59
Contributor I

Hi, I need some ECCN code for these components :

DIOtvs:2x=5V2 6V4 200p-PESD_SOT23PESD5V2S2UT
ICdig:inv=6V-74HC1GU04_TSSOP5 74HC1GU04GW,125
DIOtvs:2x=12V 14V7 75p-PESD_SOT23PESD12VS2UT
DIOtvs:2x=3V3 5V2 300p-PESD_SOT23PESD3V3S2UT
ICbus:can=5V ±58V-TJA1043_SO14TJA1043T,118
0 件の賞賛
返信
1 返信

8,799件の閲覧回数
nxf45548
NXP Employee
NXP Employee

Hi @robert59, 

Thank you for contacting NXP technical support. 
First of all, I apologize for the delay in our response. 
Following your inquiry, TJA1043T,118 is a not recommended product for new designs to get the CCN info, please send an email to [email protected] and the specialized team could further assist you. 
On the other hand, the following products do not longer belong to NXP: 

PESD5V2S2UT: Transferred to the company Nexperia on 06-Feb-2017
74HC1GU04GW,125 Transferred to Nexperia on 06-Feb-2017 
PESD12VS2UT Transferred to Nexperia on 06-Feb-2017 
PESD3V3S2UT Transferred to Nexperia on 06-Feb-2017 


For further support of these products, please contact directly with the company NEXPERIA and they will further assist you. 
Please find their contact info at the following link:
https://www.nexperia.com/about/contact-us/


Regards, 
Susi

0 件の賞賛
返信