ECC error injection info

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

ECC error injection info

1,798 次查看
veerendranathj
Contributor III

Hi,

Please provide below info..
1. Is mandatory to have test address aligned to 8 bytes? Why?

2. How it differs using Read vs Write operation to generate ECC error? 

3. How error injection will differ when I use 32-bit read/write compared to 64-bit read/write when test address not aligned to 8 bytes?

Regards,

Veeru

标记 (1)
0 项奖励
回复
1 回复

1,501 次查看
Bulat
NXP Employee
NXP Employee

1. No.

2. "Generate ECC error" can mean a) to insert an error in to the memory or b) to detect an existing error in the memory.

For a) case writes are used, for b) case reads are used.

3.

a. When ECC is enabled, the DDR controller uses only 64-bit writes.

b. If the user uses a 64-bit write, the DDR controller performs it directly.

c. If the user uses a 32-bit write, the DDR controller uses read-modify-write sequence, final write is 64-bit one as stated above. In this case "read" can potentially detect previously injected errors, so cause a ECC-related exception.

Regards,

Bulat

0 项奖励
回复