ECC algorithm of DDR SDRAM

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ECC algorithm of DDR SDRAM

ソリューションへジャンプ
2,212件の閲覧回数
yansongzhu
Contributor III

What is the ECC algorithm of DDR SDRAM on P2020 platform? It seems not the normal Hamming code.

タグ(1)
1 解決策
1,800件の閲覧回数
ufedor
NXP Employee
NXP Employee

The ECC is a (72,64) Hsiao odd-weight-column code which is modified(shortened) (127,120) Hamming code - refer to the following document (Figure 3, (c)):

https://pdfs.semanticscholar.org/dd97/ac9c9d9267793054aa38782f03342e4ccb32.pdf 

元の投稿で解決策を見る

1 返信
1,801件の閲覧回数
ufedor
NXP Employee
NXP Employee

The ECC is a (72,64) Hsiao odd-weight-column code which is modified(shortened) (127,120) Hamming code - refer to the following document (Figure 3, (c)):

https://pdfs.semanticscholar.org/dd97/ac9c9d9267793054aa38782f03342e4ccb32.pdf