Does NXP keep legacy Linux SDK's?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Does NXP keep legacy Linux SDK's?

3,723件の閲覧回数
kurt_copley
Contributor I

I need to recreate a U-Boot that was built with the gcc-4.3.74-eglibc-2.8.74/powerpc-linux-gnu/bin/powerpc-linux-gnu-gcc tool chain but have been unable to find it anywhere.

I found major and minor, but not the build version. I suspect it's custom to the NXP tool suite since the install path was /opt/freescale/usr/local/ for the defunct system I'm trying to rebuild.

Thank you.

0 件の賞賛
返信
4 返答(返信)

3,667件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Hello Kurt Copley,

This version Toolchain is provided in ISO P1020_P2020RDB_20101101_ltib.iso, I have uploaded this ISO in the following link 

https://drive.google.com/open?id=1iS3StsubAI-AumRvEHV1FEHcJnU4yvV2 

After installing this ISO and run "./ltib", toolchain gcc-4.3.74-eglibc-2.8.74 is installed in /opt/freescale/usr/local/.

Thanks,

Yiping

0 件の賞賛
返信

2,555件の閲覧回数
XKJACC
Contributor I

Hi @yipingwang ,

Could you please share it again? Google Drive is not available.

I appreciate it!

0 件の賞賛
返信

3,667件の閲覧回数
kurt_copley
Contributor I

Thank you. My employer won't allow me to download it from there. Do you know that version is still available from ltib?

0 件の賞賛
返信

3,668件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

The ltib ISO is not available in www.nxp.com.

0 件の賞賛
返信