Datalink layer and Transaction layer logic for PCIe peripheral for T2081.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Datalink layer and Transaction layer logic for PCIe peripheral for T2081.

1,130 Views
rajvad
Contributor I

Hi,

I would like to know if the Data link layer/Transaction layer logic of flow control/error control etc is present as part of the root complex controller logic itself or do these layers need to be implemented in the software. Thanks for your help.

regards,

Rajkumar

0 Kudos
Reply
1 Reply

1,110 Views
LFGP
NXP TechSupport
NXP TechSupport

The hardware related to the Data Link layer is the DPAA implemented into the SoC. You can use our SDK software that has some capabilities used in flow control.

0 Kudos
Reply