DDR3 size supported by P5040 processor

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

DDR3 size supported by P5040 processor

1,071件の閲覧回数
sanjayverma
Contributor I

Up to what size of DDR3 supported with P5040 processor?

0 件の賞賛
返信
1 返信

1,024件の閲覧回数
r8070z
NXP Employee
NXP Employee


Have a great day,

The P5040 has 2 DDR memory interfaces. Each  memory interface supports as many as four physical banks. Bank sizes up to 8 Gbytes are supported, providing up to a maximum of 32 Gbytes of DDR memory per interface.

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信